Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Power-Slide12

This is a list of parameters for a micro-power MEMS MHz and kHz clock reference. For the SiT8021, a MHz MEMS oscillator, the key take-aways are the 60µA active core current and 0.7µA standby current. The key differentiating features of the SiT1552 are a 32kHz MEMS TCXO, the active current of 1µA and the capability of driving multiple loads.

PTM Published on: 2016-04-01