Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Product List
The BBG and BBGW offer different connectivity options in order to connect with many different peripherals. However, the BBG had no wireless connectivity options onboard, and Seeed thought of making a difference by introducing the BeagleBone Green Wireless (BBGW) board. This board shares the same hardware components as the BBG, except additional connectivity options such as high performance flexible Wi-Fi and Bluetooth interfaces have been added. This makes the BBGW the first Wi-Fi/Bluetooth board of the BeagleBone family. The built-in 2.4 GHz TI WLinkTM8 Module with two antennas on the BBGW allows for the Wi-Fi and Bluetooth connectivity. Also, the onboard Ethernet port has been removed on the BBGW, and four additional USB 2.0 ports have been added on to the board.
PTM Published on: 2018-10-24