RX 12-Bit ADC

ADC-Slide1

Welcome to the Renesas RX 12-bit ADC product training module. This course contains a description of specific features of the RX 12-bit ADC, identified as S12AD in the HW manual. Additionally, it will provide an overview of the block diagram and operating modes of the ADC. There will also be a description of the channel select register and the converted value addition mode. The internal reference voltage as well as the temperature sensor will also be covered (note that neither of these are included in the RX62N). And finally there will be some helpful usage notes to aid in the application of this ADC.


PTM Published on: 2012-04-12