Step three is to confirm the high frequency characteristics of the desired relay. Isolation expresses the signal leakage level between open contacts; the larger the number, the better the leakage level will be. Insertion loss is the signal loss level between closed contacts; the smaller the number, the better the loss level is. Return loss expresses the ratio of reflected signal which occurs between the signal input and the transmission circuit; the larger the number, the lower the loss is.