Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
MCU-Slide23

The PIC24F Starter Kit is a one stop demo board for getting started with the 16-bit PIC24F. The board highlights the PIC24F USB MCU as an embedded Host, dual role, or OTG application. As an embedded host, it features firmware to interface directly to a USB Flash Drive connected to it. It also has a high resolution OLED display, touch keypad interface for user inputs, and a built in MPLAB compatible Debugger built on the board. Power to the board is provided by the PC via the USB cable.

PTM Published on: 2011-11-03