Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Inductive Ferrite Tiles

Ferrite tiles are used in wireless power charging systems to increase system efficiency, it works by shielding and reflecting the magnetic field within the inductive transfer area. The picture shown here is a good example, it shows that there are two ferrite tiles. One on the transmitter side which refers to the charging station or area, the second tile is on the receiving side which is the vehicle for this application. The ferrite tile contains the magnetic field and beams it into one direction so it is minimizing power losses, that's what happening between the two tiles. KEMET’s ferrite tiles are designed with the latest proprietary ferrite material technology to offer the highest charging efficiency.

PTM Published on: 2020-11-02