Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
ISL8117-Slide22

Another battery powered application that has seen successful implementation of the ISL8117/A is in battery-powered vehicles. Once again, the ISL8117/A is prized for its high efficiency and wide input voltage range, as well as the ease of designing it in. Battery voltages range from 24V to 48V.

PTM Published on: 2015-09-30
PTM Updated on: 2016-04-19