Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
ISL8117-Slide18

Displayed here is the circuit for the 240W design. The engineer is using an external LDO in order to boost the efficiency. If the 5V source is available, one can depopulate the LDO. The ISL8117 will automatically switch to internal LDO mode and take care of it. If the output is 5V, then just connect the output to this pin and the ISL8117 will self-bias itself from its own output.

PTM Published on: 2015-09-30
PTM Updated on: 2016-04-19