Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Product List
The C+R mode is the capacitance on the primary display and the parallel resistance R is shown on the secondary display. In AUTO mode, the Smart Tweezer first tries to perform measurement at 1 kHz and then automatically selects the best test frequency. The device is capable of measuring capacitance from approximately 3 pF to 199 μF in AUTO mode. To measure capacitance lower than 4 pF, select the 10 kHz test frequency manually. To measure capacitance higher than 200 μF, use 100 Hz or 120 Hz.
PTM Published on: 2018-12-12
PTM Updated on: 2019-02-26