Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
lr
The L+R mode is the inductance on the primary display and the series resistance on the secondary display. In AUTO mode, the Smart Tweezer automatically selects the best test frequency and is capable of measuring inductance from 1 μH to 1 kH. To measure inductance lower than 5 μH or more than 500 mH, select the test frequency manually.
PTM Published on: 2018-12-12
PTM Updated on: 2019-02-26