Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Slide3

This and the next two slides discuss how the PX3 Series Heavy Duty Pressure Transducers meet customer needs. As shown on this slide, they are efficient. The PX3 Series’ tight Total Error Band of ±1.0% FSS from -20°C to 85°C provides design engineers the most comprehensive, clear, and meaningful indication of the sensor's true measurement performance over a specified temperature range. The figure shows the possible errors of the PX3 Series, broken down by accuracy and Total Error Band. Total Error Band results in small error which promotes system efficiency and lower energy costs.

PTM Published on: 2017-01-23