Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Product List
The 1.2 A current rating is higher than the normal current rating for the rest of the Archer range, typically rated to only 1 A max.
PTM Published on: 2018-04-12
PTM Updated on: 2020-10-15