Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Product List
Powerstrate Xtreme has proven itself to be a solid solution for removing heat. This state-of-the-art phase change material has the highest thermal conductivity (3.4 W/m*K) with phase change temperature of 45°C. This material uses aluminium powder for high conductivity, so it is not electrically insulating.
PTM Published on: 2013-07-03
PTM Updated on: 2017-06-14