Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
Frame-Core-Slide8

The B82733V has a current range of 0.7 – 2.3A, an inductance range of 100 – 10mH, a stray inductance range of 2100 – 210µH, and an Rdc of 1700 – 175mΩ. Its rated current is referred to 50 Hz and the rated temperature is +40°C.

PTM Published on: 2014-03-12