Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
Frame-Core-Slide6

The B82732F has a current range of 0.45 – 1.6A, an inductance range of 100 – 10mH, a stray inductance range of 1930 – 10µH, and an Rdc of 2930 – 290mΩ. The rated current is referred to 50Hz and the rated temperature is +40°C.

PTM Published on: 2014-03-12