EC motors are capable of speed control from 10% ~ 100% of the maximum speed. Since the power required by a fan has a cubic relationship to the speed at which the fan is running there are substantial savings available by speed controlling a fan to a lower RPM. If multiple fans are set up in parallel there are large savings from speed controlling the fans instead of using on/off operation.