Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Slide13
Summarizing the results of the test, one can see that the voltage across the protected device is approximately 7 V, which is 9 V lower than the voltage across the TVS diode. One will also see that the current into the protected device is quickly reduced to about 300 mA after the initial peak of 550 mA.
PTM Published on: 2012-11-27