Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
DC-Slide8

When working with DC electronic loads, it is typical to see low and high operating ranges with their stated accuracy and resolution specifications. Accuracy and resolution is often better when operating in lower ranges than higher ranges. These operating mode accuracies are specified as a % of the programmed setting + % of the full scale rating or offset.

PTM Published on: 2013-08-19