Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Image of B&B SmartWorx/Advantech LoRaWAN® Monitoring - Alarm and Evaluation Zone

These screenshots help to visualize how the data sent by the WISE-2410 can be used to create alarms based on thresholds according to the ISO standard. For example, “Threshold 1” is for a Class 1 machine as defined by ISO 10816.

PTM Published on: 2020-11-11