Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Image of B&B SmartWorx/Advantech LoRaWAN® Monitoring - Why Condition Based Monitoring

A specialized machine requires specialized tools and technicians to maintain it. What if there was a sensor to help? When a machine’s performance begins to break down, it will typically begin to vibrate and/or heat up. The WISE-2410 helps to detect not only the vibration status but also the temperature of the machine which can reduce unscheduled maintenance and downtime by notifying operation personnel of alarm conditions. It is also able to store and visualize the machine’s vibration and temperature data.

PTM Published on: 2020-11-11