Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Guide to PCB Layout Slide 18

Capacitor Resistances are RS and RP. RS is the ESR of the cap and it is the combined equivalent of RS and RP this is the AC resistance of the cap. RP is the insulation resistance of the cap, it is a measure of the amount of DC current that flows through the dielectric of a cap with a voltage applied. RP is typically 100,000M ohms or more. And RDA and CDA represent the capacitors dielectric absorption.

PTM Published on: 2007-01-30