Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Package and Pinout

The A17700 uses a QFN package, 4 x 4 mm, with 24 pins. It is a small package ideal if there is a space constraint in the system. The A17700 also offers higher reliability with redundant pins to the supply and ground bridge connections.

PTM Published on: 2021-04-07