Transistors Basics: MOSFET
2024-09-30 | By Alex Nguyen
A transistor is a type of semiconductor device that can conduct and insulate electric current or voltage. It can act as an amplifier or a switch. There are many different types of transistors, the majority of which can be split into the following diagram:
Figure 1 Different Types of Transistors.
What is a MOSFET?
MOSFET stands for “metal-oxide-semiconductor field-effect transistor.” The general layout of their structure is that they have a source, drain, gate, and body, also referred to as substrate. MOSFETs are split into two types: n-channel and p-channel.
- N-channel MOSFET, also known as NMOS or NFET, creates a current channel between the source and the drain when a positive voltage vGS is applied between the gate and the source.
- P-channel MOSFET, also called PMOS or PFET, creates a current channel between the source and the drain when a negative voltage vGS is applied between the gate and source.
When the voltage at the source is equal to the voltage at the body, then the MOSFET can be represented without the body.
What is a MOSFET Made Out of?
The physical structure of an NMOS and PMOS is similar but differs in the semiconductor material used:
- NMOS: The body is made of p-type substrate. The source and drain are heavily doped with n-type material.
- PMOS: The body is made of n-type substrate. The source and drain are heavily doped with p-type material.
Figure 2 Physical Structure of NMOS and PMOS.
Focusing on the NMOS structure, “the transistor is built on a p-type substrate, a single-crystal silicon wafer that provides physical support for the device.” As indicated by n+, the heavily doped n-type source and drain are created in the substrate. Afterwards, a thin layer of silicon dioxide (SiO2) which typically varies in thickness tox from 1nm to 10nm, is grown on the surface of the substrate. SiO2 is an amazing insulator, so it covers the area between the source and drain. Metal is then deposited onto the silicon dioxide layer to form the gate of the transistor. “Metal contacts are also made to the source region, the drain region, and the substrate.”
Figure 3 Physical Structure of NMOS in Perspective View.
How Does MOSFET Operate?
Current Channel
For NMOS, when zero voltage is applied to the gate, it is like having “two back-to-back diodes in series between drain and source.” For PMOS, if a high voltage is applied to the gate, the diode configuration would be the reverse. This situation makes it difficult for the transistor to conduct current between the source and drain. “The path between drain and source has a very high resistance (of the order of 1012 Ω)”.
Figure 4 MOSFET Zero Gate Voltage Diode Configuration.
For NMOS, the source and drain are grounded before a positive voltage vGS is applied to the gate. Since the other terminals are grounded, the positive gate voltage causes holes (positively charged) in the substrate beneath the gate to be repelled, leaving behind a depletion region. This depletion region is left with a net positive charge, making it more susceptible to electrons (negative charge). “The positive gate voltage attracts electrons from the n^+ source and drain regions (where they are in abundance) into the channel region.” After enough electrons gather in the substrate under the gate, an n-channel is created, connecting the source and drain. When a voltage is applied between the source and drain, this induced region allows current to flow. The voltage vGS required to create a conducting channel under the gate is called the threshold voltage, Vt. Typically, the value of Vt lies between 0.3V to 1V.
Figure 5 NMOS with Current Channel.
For PMOS, a channel between the source and drain that allows current to flow is created when a negative voltage is applied to the gate vGS. When the magnitude of the negative vGS is “beyond the magnitude of the threshold voltage Vt, which by convention is negative, a p-channel is established.”
Figure 6 PMOS with Current Channel.
Channel Conductance
There are three factors that control NMOS channel conductance: μnCox, (W/L), and vOV. “The first factor is determined by the process technology used to fabricate the MOSFET. μn represents electron mobility, which is how easily electrons can move on the surface of the channel. Cox“ is the capacitance of the parallel-plate capacitor per unit gate area. The product μnCox“ is called process transconductance parameter and given the symbol kn'.” The second factor is the transistor aspect ratio (W/L). “W is the width of the channel, and L is the length of the channel”. This aspect ratio is dictated by the device designer, “who can select the values of W and L to give the device the i−v characteristics desired”. In 2019, the minimum channel length was 14 nm. The third term is the overdrive voltage vOV, sometimes referred to as vGS-Vt. This voltage determines the amount of electron charge in the channel, which directly influences MOSFET’s conductance.
PMOS almost has the same three factors that contribute to the channel conductance. The difference is the process transconductance parameter kp' is represented by μpCox. μp represents hole mobility, which is how easily holes can move on the surface of the channel. Cox and (W/L) remain the same from NMOS. To have the correct polarity, overdrive voltage vOV is sometimes referred to as vSG-Vt.
Operational Regions
There are two main operation regions for NMOS: triode and saturation. Each region has different characteristics and equations governing the current. The triode region happens when vGD>Vt or vDS<vOV where the current channel is formed. When vDS is small, the current is proportional to vOV . “As vDS increased, the channel becomes more tapered, and its resistance increases correspondingly” causing the increase in current to slow down. The saturation region happens when vGD≤Vt or vDS≥vOV . The “current saturates because the channel is pinched off at the drain end, and vDS no longer affects the channel”.
Figure 7 NMOS Drain Current.
PMOS has similar regions to NMOS, which are triode and saturation. There are slight differences in the operation and condition. The triode region is obtained by vGD>|Vt|or vSD<|vOV|. The saturation region is obtained by vDG≤|Vt| or vSD≥|vOV|.
Figure 8 PMOS Drain Current.
Further Reading
To get an understanding of BJT (Bipolar Junction Transistor), further reading can be completed here.
Reference
“Transistor - Definition, Working Principle, Types, Transistor Diagram,” BYJUS. https://byjus.com/jee/transistor/
Adel Sedra, K. C. Smith, Tony Chan Carusone, and V. Gaudet, Microelectronic Circuits. 2019.
“The Significance of the Intrinsic Body Diodes Inside MOSFETs,” DigiKey, Sep. 22, 2016. https://www.digikey.com/en/articles/the-significance-of-the-intrinsic-body-diodes-inside-mosfets
Related Content
Transistor Basics: NPN & PNP Using 2N3904, 2N3906, 2N2222, and 2N2907
The Significance of the Intrinsic Body Diodes Inside MOSFETs
How to Select a MOSFET for Logic Circuits or Gate Design
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.