制造商零件编号 4950
ADAFRUIT METRO M7 WITH AIRLIFT -
Adafruit Industries LLC
License: See Original Project
Courtesy of Adafruit
Guide by John Park
Overview
When PT discovered this beautiful artifact from 1979, the Computer Perfection electronic memory game, we knew we had to transform it into a sci-fi drone synthesizer!
Luckily, this coincided with Jepler's work on the CircuitPython synthio library and the release of the Metro M7 -- a perfect confluence of events!
This project takes the Computer Perfection and reuses its buttons and switches to trigger a polyphonic, multi-timbral wavetable synthesizer for all your spacey jam sessions. It includes ADSR envelopes and LFO modulation for a beautiful, other-worldly sound.
Parts
28-position DIP Connector You'll use this to wire the buttons and switches to the Metro M7 using the original DIP socket.
1 x Clear Adhesive Squares
Install CircuitPython
CircuitPython is a derivative of MicroPython designed to simplify experimentation and education on low-cost microcontrollers. It makes it easier than ever to get prototyping by requiring no upfront desktop software downloads. Simply copy and edit files on the CIRCUITPY drive to iterate.
CircuitPython QuickStart
Follow this step-by-step to quickly get CircuitPython running on your board.
Download the latest version of CircuitPython for this board via circuitpython.org
Click the link above to download the latest CircuitPython UF2 file.
Save it wherever is convenient for you.
Plug your board into your computer, using a known-good data-sync cable, directly, or via an adapter if needed.
Click the reset button once (highlighted in red above), and then click it again when you see the RGB status LED(s) (highlighted in green above) turn purple (approximately half a second later). Sometimes it helps to think of it as a "slow double-click" of the reset button.
On some very old versions of the UF2 bootloader, the status LED turns red instead of purple.
Once successful, you will see the RGB status LED(s) turn green (highlighted in green above). If you see red, try another port, or if you're using an adapter or hub, try without the hub, or different adapter or hub.
If double-clicking doesn't work the first time, try again. Sometimes it can take a few tries to get the rhythm right!
A lot of people end up using charge-only USB cables and it is very frustrating! Make sure you have a USB cable you know is good for data sync.
You will see a new disk drive appear called METROM7BOOT.
Drag the adafruit_circuitpython_etc.uf2 file to METROM7BOOT.
The BOOT drive will disappear, and a new disk drive called CIRCUITPY will appear.
That's it!
Code the Computer Perfection Synth
Text Editor
Adafruit recommends using the Mu editor for editing your CircuitPython code. You can get more info in this guide.
Alternatively, you can use any text editor that saves simple text files.
Download the Project Bundle
Your project will use a specific set of CircuitPython libraries, and the code.py file. To get everything you need, click on the Download Project Bundle link below, and uncompress the .zip file.
Connect your computer to the M7 board via a known good USB power+data cable. A new flash drive should show up as CIRCUITPY.
Drag the contents of the uncompressed bundle directory onto your board's CIRCUITPY drive, replacing any existing files or directories with the same names, and adding any new ones that are necessary.
# SPDX-FileCopyrightText: 2023 John Park, Jeff Epler, and Tod Kurt for Adafruit Industries
# SPDX-License-Identifier: MIT
# Computer Perfection Synth
# * 10 numbered buttons play notes
# * SET button to increase LFO rate, long press to decrease LFO rate
# * SCORE button to add lower octave
# * MODE switch changes wavetable set
# * SKILL switch toggles sustain
# * GAME switch must stay in position 1 or it messes with the other switches
import time
import random
import board
import audiobusio
import audiomixer
import synthio
import ulab.numpy as np
import neopixel
import keypad
# NeoPixel setup
num_pixels = 34
pixels = neopixel.NeoPixel(board.D11, num_pixels, brightness=0.7, auto_write=False)
pixels.fill(0x0)
pixels.show()
time.sleep(0.25)
pix_map = [26, 23, 19, 16, 13, 10, 7, 4, 32, 29] # map the LEDs to the numbered panel sections 0-9
for p in range(len(pix_map)):
pixels[pix_map[p]] = 0xff0000
pixels.show()
time.sleep(0.1)
note_buttons = keypad.Keys(
(board.D0, board.D1, board.D2, board.D3, board.D4,
board.D5, board.D6, board.D7, board.D8, board.A5),
value_when_pressed=False,
pull=True
)
switches = keypad.Keys(
(board.A1, board.A0),
value_when_pressed=False,
pull=True
)
octave = 3 # octave multiplier
note_list = (0, 4, 6, 7, 9, 12, 16, 18, 19, 21) # Lydian scale
mod_buttons = keypad.Keys(
(board.A4, board.A3), # SET and SCORE buttons
value_when_pressed=False,
pull=True
)
SAMPLE_RATE = 48000 # clicks @ 36kHz & 48kHz on rp2040
SAMPLE_SIZE = 200
VOLUME = 12000
# Metro M7 pins for the I2S amp:
lck_pin, bck_pin, dat_pin = board.D9, board.D10, board.D12
# synth engine setup
waveform = np.zeros(SAMPLE_SIZE, dtype=np.int16) # intially all zeros (silence)
amp_env = synthio.Envelope( # default (0.1, 0.05, 0.2, 1, 0.8)
attack_time=1.0,
decay_time=0.05,
release_time=3.0,
attack_level=1.0,
sustain_level=0.8
)
synth = synthio.Synthesizer(sample_rate=SAMPLE_RATE, waveform=waveform, envelope=amp_env)
audio = audiobusio.I2SOut(bit_clock=bck_pin, word_select=lck_pin, data=dat_pin)
mixer = audiomixer.Mixer(voice_count=1, sample_rate=SAMPLE_RATE, channel_count=1,
bits_per_sample=16, samples_signed=True, buffer_size=8192)
audio.play(mixer)
mixer.voice[0].level = 0.55
mixer.voice[0].play(synth)
led = neopixel.NeoPixel(board.NEOPIXEL, 1, brightness=0.3) # on board neopixel
# waveforms setup
wave_sine = np.array(np.sin(np.linspace(0, 2*np.pi, SAMPLE_SIZE, endpoint=False)) * VOLUME,
dtype=np.int16)
wave_saw = np.linspace(VOLUME, -VOLUME, num=SAMPLE_SIZE, dtype=np.int16)
wave_weird1 = np.array((198,2776,5441,8031,10454,12653,14609,16333,17824,19130,20260,21227,22043,
22721,23269,23699,24019,24243,24385,24461,18630,-26956,-28048,-29175,-30249,
-31227,-32073,-32631,-32359,-31817,-30941,-29663,-27900,-25596,-22591,
-18834,-14291,-9016,-3212,2794,8624,13943,18544,22353,25408,27780,29553,
30855,31751,32315,32611,32687,32593,32351,31983,31491,30871,30097,28895,
-28240,-30489,-31343,-31975,-32431,-32697,-32767,-32615,-32217,-31525,
-30489,-29035,-27090,-24519,-21237,-17178,-12339,-6829,-902,5081,10748,
15805,20102,23615,26396,28510,30109,31245,31995,31955,31437,30729,29887,
28943,27908,26784,25560,24077,22781,-22207,-22735,-22709,-22471,-22065,
-21497,-20773,-19896,-18872,-17698,-16361,-14857,-13141,-11206,-9054,-6717,
-4259,-1796,522,2548,4167,5339,6079,6445,6503,6319,5949,5449,4847,4183,
3480,2756,2028,1304,590,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,
0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,-478,-1168,-1882,-2596,
-3336,-4074,-4795,-5487,-6119,-6669,-7095,-7357,-7399,-7157,-6559,-5543,
-4076,-2132,), dtype=np.int16)
wave_noise = np.array([random.randint(-VOLUME, VOLUME) for i in range(SAMPLE_SIZE)], dtype=np.int16)
# map s range a1-a2 to b1-b2
def map_range(s, a1, a2, b1, b2):
return b1 + ((s - a1) * (b2 - b1) / (a2 - a1))
# mix between values a and b, works with numpy arrays too, t ranges 0-1
def lerp(a, b, t):
return (1-t)*a + t*b
waveform[:] = wave_saw
wave_mix = 0.0
lfo_rates = (0.1, 0.5, 0.8, 1.5, 3.0, 6.0, 7.0, 8.0)
lfo_index = 0
lfo1 = synthio.LFO(rate=(lfo_rates[lfo_index]), waveform=wave_sine) # rate is in Hz
synth.lfos.append(lfo1)
hold = False # state of note hold
octaves = False
def light_button_pixels(button_number):
pixels[pix_map[button_number]+1] = 0xFF0000
pixels[pix_map[button_number]-1] = 0xFF0000
pixels.show()
def reset_button_pixels(button_number):
pixels[pix_map[button_number]+1] = 0x000000
pixels[pix_map[button_number]-1] = 0x000000
pixels.show()
def clamp(v, low, high):
return min(max(v, low), high)
print("-Computer Perfection Synth-")
note = None
mod_key = 0
last_mod_button_event_time = 0
waveset = 0
while True:
# watch for mod buttons to be pressed
mod_button_event = mod_buttons.events.get()
if mod_button_event:
mod_key = mod_button_event.key_number
if mod_button_event.pressed:
if mod_key == 0: # SET switch
last_mod_button_event_time = time.monotonic()
if mod_key == 1: # enable octaves
octaves = True
if mod_button_event.released:
if last_mod_button_event_time and mod_key == 0: # short press-release increase LFO rate
lfo_index = clamp(lfo_index+1, 0, len(lfo_rates)-1)
print(lfo_index)
lfo_rate = lfo_rates[lfo_index]
lfo1.rate = lfo_rate
last_mod_button_event_time = 0
if mod_key == 1: # disable octaves
octaves = False
# long press slows the LFO rate
if last_mod_button_event_time != 0 and time.monotonic() - last_mod_button_event_time > 1.0:
last_mod_button_event_time = 0
lfo_index = clamp(lfo_index-1, 0, len(lfo_rates)-1)
lfo_rate = lfo_rates[lfo_index]
lfo1.rate = lfo_rate
# watch for note buttons to be pressed
note_button_event = note_buttons.events.get()
if note_button_event:
i = note_button_event.key_number
if note_button_event.pressed:
if octaves:
synth.press((note_list[i]+(octave*12), note_list[i]+(octave*12)-12))
else:
synth.press((note_list[i]+(octave*12),))
light_button_pixels(i)
if note_button_event.released:
if not hold:
reset_button_pixels(i)
synth.release((note_list[i]+(octave*12), note_list[i]+(octave*12)-12))
reset_button_pixels(i)
# watch for switches to be changed
switch_event = switches.events.get()
if switch_event:
sw = switch_event.key_number
if switch_event.pressed:
if sw == 0: # MODE toggle right
mixer.voice[0].level = 0.45
# wave_mix = 0.5
waveset = 0
if sw == 1: # SKILL toggle center
hold = True
if switch_event.released:
if sw == 0: # MODE toggle center
mixer.voice[0].level = 0.95
waveset = 1
if sw == 1: # SKILL toggle right or left
hold = False
for r in range(len(note_list)): # turn off all notes
# if octaves:
synth.release((note_list[r]+(octave*12), note_list[r]+(octave*12)-12))
for h in range(len(pix_map)): # turn off held pixels
reset_button_pixels(h)
lfo_val_for_lerp = map_range(lfo1.value, -1, 1, 0, 1)
if waveset == 0:
waveform[:] = lerp(wave_sine, wave_weird1, lfo_val_for_lerp)
else:
waveform[:] = lerp(wave_saw, wave_noise, lfo_val_for_lerp)
How it Works
Libraries
First, we import the required libraries:
import time
import random
import board
import audiobusio
import audiomixer
import synthio
import ulab.numpy as np
import neopixel
import keypad
NeoPixels
Next we initialize the NeoPixel strip with 34 pixels connected to pin D11 on the board.
We also set up a list of the physical pixels that correspond to the game panel's 0-9 locations.
# NeoPixel setup
num_pixels = 34
pixels = neopixel.NeoPixel(board.D11, num_pixels, brightness=0.7, auto_write=False)
pixels.fill(0x0)
pixels.show()
time.sleep(0.25)
pix_map = [26, 23, 19, 16, 13, 10, 7, 4, 32, 29] # map the LEDs to the numbered panel sections 0-9
for p in range(len(pix_map)):
pixels[pix_map[p]] = 0xff0000
pixels.show()
time.sleep(0.1)
Keypad
We'll use the keypad library to read the ten note buttons, two modifier buttons, and two switches.
note_buttons = keypad.Keys(
(board.D0, board.D1, board.D2, board.D3, board.D4,
board.D5, board.D6, board.D7, board.D8, board.A5),
value_when_pressed=False,
pull=True
)
switches = keypad.Keys(
(board.A1, board.A0),
value_when_pressed=False,
pull=True
)
mod_buttons = keypad.Keys(
(board.A4, board.A3), # SET and SCORE buttons
value_when_pressed=False,
pull=True
)
Notes
The synthio library can use MIDI note numbers or frequency to specify a note to play. In this project we'll use MIDI note numbers as they're easier to adjust for interval/scale choices.
This note_list contains the ten notes we'll play, and the octave variable specifies which octave to play them in.
octave = 3 # octave multiplier
note_list = (0, 4, 6, 7, 9, 12, 16, 18, 19, 21) # Lydian scale
I2S Amp
The I2S amp is set up on three pins of the Metro M7 (this can vary for other boards.)
lck_pin, bck_pin, dat_pin = board.D9, board.D10, board.D12
Synth Setup
The synthio object is set up with the sample rate, sample size, volume, initial waveform, and audiobus/audiomixer objects.
SAMPLE_RATE = 48000 # clicks @ 36kHz & 48kHz on rp2040
SAMPLE_SIZE = 200
VOLUME = 12000
# synth engine setup
waveform = np.zeros(SAMPLE_SIZE, dtype=np.int16) # intially all zeros (silence)
amp_env = synthio.Envelope( # default (0.1, 0.05, 0.2, 1, 0.8)
attack_time=1.0,
decay_time=0.05,
release_time=3.0,
attack_level=1.0,
sustain_level=0.8
)
synth = synthio.Synthesizer(sample_rate=SAMPLE_RATE, waveform=waveform, envelope=amp_env)
audio = audiobusio.I2SOut(bit_clock=bck_pin, word_select=lck_pin, data=dat_pin)
mixer = audiomixer.Mixer(voice_count=1, sample_rate=SAMPLE_RATE, channel_count=1,
bits_per_sample=16, samples_signed=True, buffer_size=8192)
audio.play(mixer)
mixer.voice[0].level = 0.55
mixer.voice[0].play(synth)
Waveforms
Different waveforms have different harmonics, which is what provides the "character" or timbre of an instrument. We'll use sine, saw, the weird1 wavetable, and noise waveforms, which can be mixed between using the LFO modulator.
All of these waveforms are defined mathematically, except for the weird1 which is defined with an array of discreet points.
# waveforms setup
wave_sine = np.array(np.sin(np.linspace(0, 2*np.pi, SAMPLE_SIZE, endpoint=False)) * VOLUME,
dtype=np.int16)
wave_saw = np.linspace(VOLUME, -VOLUME, num=SAMPLE_SIZE, dtype=np.int16)
wave_weird1 = np.array((198,2776,5441,8031,10454,12653,14609,16333,17824,19130,20260,21227,22043,
22721,23269,23699,24019,24243,24385,24461,18630,-26956,-28048,-29175,-30249,
-31227,-32073,-32631,-32359,-31817,-30941,-29663,-27900,-25596,-22591,
-18834,-14291,-9016,-3212,2794,8624,13943,18544,22353,25408,27780,29553,
30855,31751,32315,32611,32687,32593,32351,31983,31491,30871,30097,28895,
-28240,-30489,-31343,-31975,-32431,-32697,-32767,-32615,-32217,-31525,
-30489,-29035,-27090,-24519,-21237,-17178,-12339,-6829,-902,5081,10748,
15805,20102,23615,26396,28510,30109,31245,31995,31955,31437,30729,29887,
28943,27908,26784,25560,24077,22781,-22207,-22735,-22709,-22471,-22065,
-21497,-20773,-19896,-18872,-17698,-16361,-14857,-13141,-11206,-9054,-6717,
-4259,-1796,522,2548,4167,5339,6079,6445,6503,6319,5949,5449,4847,4183,
3480,2756,2028,1304,590,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,
0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,-478,-1168,-1882,-2596,
-3336,-4074,-4795,-5487,-6119,-6669,-7095,-7357,-7399,-7157,-6559,-5543,
-4076,-2132,), dtype=np.int16)
wave_noise = np.array([random.randint(-VOLUME, VOLUME) for i in range(SAMPLE_SIZE)], dtype=np.int16)
waveform[:] = wave_saw
wave_mix = 0.0
Low Frequency Oscillator
A low frequency oscillator, or LFO, is a waveform with a frequency below the audible threshold. LFOs are often used to modulate other synthesizer parameters, such as the pitch or amplitude of an audio oscillator's waveform.
We'll run an LFO at different rates by pressing the SET button to cycle among them in the lfo_rates list.
The lfo1 object is created with a rate and waveshape, in this case a sine, but this could be any shape you like, such as a triangle or saw.
lfo_rates = (0.1, 0.5, 0.8, 1.5, 3.0, 6.0, 7.0, 8.0)
lfo_index = 0
lfo1 = synthio.LFO(rate=(lfo_rates[lfo_index]), waveform=wave_sine) # rate is in Hz
synth.lfos.append(lfo1)
Helper Functions
We create a number of helper functions to control NeoPixels when buttons are pressed, remap and clamp values, and provide linear interpolation (lerp) between values.
# map s range a1-a2 to b1-b2
def map_range(s, a1, a2, b1, b2):
return b1 + ((s - a1) * (b2 - b1) / (a2 - a1))
# mix between values a and b, works with numpy arrays too, t ranges 0-1
def lerp(a, b, t):
return (1-t)*a + t*b
def light_button_pixels(button_number):
pixels[pix_map[button_number]+1] = 0xFF0000
pixels[pix_map[button_number]-1] = 0xFF0000
pixels.show()
def reset_button_pixels(button_number):
pixels[pix_map[button_number]+1] = 0x000000
pixels[pix_map[button_number]-1] = 0x000000
pixels.show()
def clamp(v, low, high):
return min(max(v, low), high)
Main Loop
The main loop of the program checks for button presses and switch events.
When a note button is pressed a corresponding synth note is played (and the NeoPixels surrounding the button position light up). You'll notice the notes have a short attack and a long release, thanks to the ADSR envelope values we created initially.
If the SCORE button is held, the note buttons will also play a unison note one octave down.
Pressing the SET button increments the LFO rate, while a long press decrements it.
Flipping the MODE switch changes the waveform pair that's mixed between.
When the SKILL switch is in the center position, all pressed notes will sustain indefinitely -- perfect for nice drone chords! In the non-center positions the notes will release when the note buttons are released.
# watch for mod buttons to be pressed
mod_button_event = mod_buttons.events.get()
if mod_button_event:
mod_key = mod_button_event.key_number
if mod_button_event.pressed:
if mod_key == 0: # SET switch
last_mod_button_event_time = time.monotonic()
if mod_key == 1: # enable octaves
octaves = True
if mod_button_event.released:
if last_mod_button_event_time and mod_key == 0: # short press-release increase LFO rate
lfo_index = clamp(lfo_index+1, 0, len(lfo_rates)-1)
print(lfo_index)
lfo_rate = lfo_rates[lfo_index]
lfo1.rate = lfo_rate
last_mod_button_event_time = 0
if mod_key == 1: # disable octaves
octaves = False
# long press slows the LFO rate
if last_mod_button_event_time != 0 and time.monotonic() - last_mod_button_event_time > 1.0:
last_mod_button_event_time = 0
lfo_index = clamp(lfo_index-1, 0, len(lfo_rates)-1)
lfo_rate = lfo_rates[lfo_index]
lfo1.rate = lfo_rate
# watch for note buttons to be pressed
note_button_event = note_buttons.events.get()
if note_button_event:
i = note_button_event.key_number
if note_button_event.pressed:
if octaves:
synth.press((note_list[i]+(octave*12), note_list[i]+(octave*12)-12))
else:
synth.press((note_list[i]+(octave*12),))
light_button_pixels(i)
if note_button_event.released:
if not hold:
reset_button_pixels(i)
synth.release((note_list[i]+(octave*12), note_list[i]+(octave*12)-12))
reset_button_pixels(i)
# watch for switches to be changed
switch_event = switches.events.get()
if switch_event:
sw = switch_event.key_number
if switch_event.pressed:
if sw == 0: # MODE toggle right
mixer.voice[0].level = 0.45
# wave_mix = 0.5
waveset = 0
if sw == 1: # SKILL toggle center
hold = True
if switch_event.released:
if sw == 0: # MODE toggle center
mixer.voice[0].level = 0.95
waveset = 1
if sw == 1: # SKILL toggle right or left
hold = False
for r in range(len(note_list)): # turn off all notes
# if octaves:
synth.release((note_list[r]+(octave*12), note_list[r]+(octave*12)-12))
for h in range(len(pix_map)): # turn off held pixels
reset_button_pixels(h)
lfo_val_for_lerp = map_range(lfo1.value, -1, 1, 0, 1)
if waveset == 0:
waveform[:] = lerp(wave_sine, wave_weird1, lfo_val_for_lerp)
else:
waveform[:] = lerp(wave_saw, wave_noise, lfo_val_for_lerp)
Assemble the Computer Perfection Synth
Open the Panel
Remove the two screws at the bottom of the top panel, then pivot the panel open.
Remove PCB
Unscrew the four screws holding the game PCB in place.
Desolder Wires
Desolder the two lid switch wires, as well as the two piezo buzzer wires.
Remove Microcontroller
The Computer Perfection game ran on a 4-bit microcontroller, the Matsushita MN1400ML.
Carefully pry it up to remove it from the DIP socket. We won't be re-using the chip, but we will use the socket to connect all of the buttons and switches to our Metro M7. A rather large upgrade!
Wiring Diagram
The Fritzing diagram and schematic below show the connections we'll make to use the Computer Perfection game's buttons and switches as GPIO inputs on the Metro M7.
You can also see the connections to the I2S amplifier and NeoPixels.
DIP Header Wiring
Rather than tediously solder wires to the underside of the board, we'll use this super cool DIP header that Jan Goolsbey suggested.
These are designed to clamp down on flat ribbon wires, but in this case, we'll use silicone sheathed wire for the necessary flexibility and low profile that'll allow the wire bundle to be routed out and under the board.
A pair of tweezers works well for pressing each wire into its pin slot -- no need to remove insulation, the pin does the work for you.
Using the Fritzing diagram as a guide, run each wire to its respective pad on the Proto-Screwshield.
Cap
Press the connector's cap into place.
Socket Connection
Paying attention to the orientation, place the DIN connector in the DIP socket, being careful to seat each leg so that nothing is misaligned or bent.
Use tape to neatly dress the wiring off to the left side of the board.
Wiring Length
Remount the PCB to the Computer Perfection top panel so you can pull the wires to even length in the Proto-Screwshield.
Remove a bit of the insulation and solder each wire.
I2S Amp
To prep the I2S amp, first solder the header strip and terminal block as shown here.
Solder a 7-pin section of socket header pins to the proto area of the Proto-Screwshield.
Run wires to pins D9, D10, D12, GND, and 3.3V as shown to correspond with the pins of the amplifier, connecting them to their respective pins on the headers.
Feed the speaker wires through the base and screw them into the terminal block.
Plug the amplifier into the board.
Mount Speaker
Use a piece of double-stick foam tape to mount the speaker in the base as shown.
NeoPixel Wiring
We can't re-use the existing LEDs on the board easily because they are wired to the same pins as the input buttons -- the original microcontroller pins toggled quickly between input and output to perform both functions -- so we'll upgrade the Computer Perfection with a strip of NeoPixels!
Solder terminal blocks to the Proto-Screwshield to accommodate the NeoPixel wiring to pin D11, GND, and 3.3V.
LED Placement
Remove the PCB and test fit the NeoPixel strip, then cut off the excess as shown.
Use the uGlu dashes or other adhesive to affix the NeoPixels, running the wiring to the side as shown.
Put the PCB back onto the top panel.
Screw the NeoPixel wires into their blocks and then you can plug the Proto Screwshield into the Metro M7.
USB Cable
Assemble the DIY USB cable USB-C end to the ribbon cable and plug it into the Metro M7.
Run the ribbon through the base as shown, then attach the micro-B socket.
Metro Placement
Use double-stick foam tape to adhere the Metro M7 to the inner base, then screw the top panel into place.
Magnetic USB Cable
You can optionally use a magnetic tipped USB cable to make the connections a bit easier.
Play the Computer Perfection Synth
Playing the Computer Perfection synthesizer is satisfying and simple! There are just a few options to know about:
Press any blue button to play a note. You can play multiple notes at once to create chords.
If the Sustain (SKILL) switch is in position 3 or 1, the note will only sustain as long as you hold the button or buttons.
Move the Sustain (SKILL) switch to the center position marked 2 and any new notes will drone indefinitely until you move the switch to the left or right.
Hold the Sub-Octave (SCORE) button to add an additional note one octave below any new notes you play.
Press and release the green LFO (SET) button to increase the LFO rate by one step in the rate list. Long-press (about a second) it to decrease the LFO rate by one step.
Set the Waveform (MODE) switch to the center for one waveset or to the right for the other -- the wavesets contain two mixed waveforms that the LFO modulates between.
Leave the GAME switch in the left-most position otherwise the other switches and buttons will misbehave.