Maker.io main logo

Projects

PROJECT

Changing Bootloader on a Nano using a Custom Shield

By PTSolns

This tutorial shows the steps to change bootloader (old and new) on the Nano development board using a custom shield and an Uno as the programmer.

PROJECT

Making a Simple RF Network

By PTSolns

A simple getting started project demonstrating one-way RF communication between two nodes using the NRF-Shield.

PROJECT

Custom 24-Hour Single Revolution Clock

By PTSolns

A custom 24-hour single revolution clock made with an RTC and a stepper motor, controlled by the Nano Flip, all put together on the Proto-Half.

PROJECT

The Nano That Wanted to Be an Uno

By PTSolns

At the end of the project, you'll get a Nano that has a footprint of the Uno.

PROJECT

Adjustable Resistive Load for 5 VDC 1000 mA Applications

By PTSolns

An adjustable resistive load is developed with parts commonly found in most home and professional labs. The load can be adjusted to yield a range of current draws. This tool can be used to test, for example, the stable region of voltage regulators or other power management circuitry.