Using Infrared Technology for Sensing
投稿人:DigiKey
2012-02-23
Introduction
Infrared (IR) technology addresses a broad variety of wireless applications, especially in the areas of sensing and remote control. Today’s newest products, such as cell phones, digital cameras, and DVD players as well as remote controls for every market segment, rely on IR sensing and control devices. For more than 40 years, ROHM Semiconductor has been driving technology advances that have led to a growing number of IR sensing and communication applications.
About optical sensors
To understand infrared technology, the best starting point is the electromagnetic spectrum. The frequency range and wavelengths of the entire spectrum are shown in Figure 1. The IR portion of the electromagnetic spectrum is usually divided into three regions: the near-, mid- and far- infrared. The wavelengths for these regions are shown in Table 1. Infrared wavelengths range from red to violet. The frequencies are higher than microwave but shorter than visible light.
Focusing on near-infrared devices and applications, PhotoOptic technologies are used for optical sensing and optical communications with numerous general market applications, since light is less complex than RF when implemented as the signal source. Optical sensors are used in industrial, consumer and other applications for sensing movement, position, proximity, ambient light, speed, and direction.
Figure 1: Infrared signals are near the middle of the electromagnetic spectrum, above radio and well below gamma ray.
IR-A: 700 nm–1400 nm (0-7 µm – 1.4 µm) | Near - fiber optic, IR sensors |
IR-B: 1400 nm–3000 nm (1.4 µm – 3 µm) | Mid - heat sensing |
IR-C: 3000 nm–1 mm (3 µm – 1000 µm) | Far - thermal imaging |
Table 1: Wavelengths and frequencies for the IR spectrum.
Optical wireless communication uses IR data transmission for short range applications, such as computer peripherals and PDAs (personal digital assistants). For optical communication, a modulated IR light beam transmitted by an emitter LED is received by a silicon photodiode. Infrared Data Association (IrDA) standards provide the protocol for these types of communication. Since IR does not penetrate walls, it does not interfere with other signals in indoor environments. IR technology is the most commonly used technique for remotely controlling appliances.
Some general applications for IR components include:
- Office Automation (OA) equipment such as copiers, fax machines, and printers
- Vending machines
- Gaming products
- Home entertainment products
- Medical / health care equipment
- Banking terminals such as ATMs
- Testing equipment such as IC/LSI testers, encoders, and more
To address the variety of sensing applications, products take advantage of several IR technologies including:
- IR Emitters
- IR Receivers (sensors)
- Photointerrupters and Photo Reflectors
- Tilt Sensors
- IrDA Communication Modules
- Remote Control Module Receivers
A brief explanation of each shows the commonalities and differences.
An IR Emitter is a light emitting diode (LED). Different types of IR LEDs are specified based on their packaging.IR Receivers are also called sensors since they detect the wavelength and spectral radiation of the light from the IR emitter. IR receivers are specified by optic features, packaging, special circuitry such as an ambient light filter, wide viewing angle, and more.
A photointerrupter is a photosensor that integrates an optical receiver and emitter in a single U-shaped package. In a transmission type photointerrupter, the light emitting and detecting elements are placed facing each other (Figure 2). Shape and size are two of the main differentiating features of a photointerrupter.
As shown in Figure 3, product characteristics are determined by the slit and gap - the width or distance from emitter to receiver/sensor. The vertical or horizontal slit width is the window opening for collimating, also called the beam width. Besides the slit and gap, additional selection criteria include the output type, such as analog, digital, and dual-phase output signals. Typical applications include printers, counters, opto encoders, directional movement detection, and more.
Figure 3: Photointerrupters are specified by gap and slit dimensions as well as outputs.
Photo reflectors or reflective type sensors are side-by-side emitter-sensor (photointerrupter) devices that detect reflected beams from a surface. Figure 4 shows a typical photo reflector design. Key electrical characteristics include the following: transfer gain rate, sensor collector current vs. IR LED current, wavelength, and response switching time. Reflective type sensors can be used in proximity sensing applications.
Figure 4: Reflective type photo sensors detect light reflected by a target object.
Tilt sensors represent a special type of sensing design for PhotoOptics. Figure 5 shows image rotation as part of the sensing commonly used in portable products with displays, such as cameras and cell phones.
Figure 5: With careful design consideration, optical tilt sensors can provide four-direction detection. Source: ROHM Semiconductor.
IrDA communication modules used in local networks have three different forms:
- IrDA-SIR (slow speed) infrared supporting data rates up to 115 Kbps
- IrDA-MIR (medium speed) infrared supporting data rates up to 1.15 Mbps
- IrDA-FIR (fast speed) infrared supporting data rates up to 4 Mbps
Remote control module receivers operate at a variety of carrier frequencies (typically in the 30 to 60 kHz range). Units with a dual lens provide a higher degree and wider range of sensitivity. The small size and (typical) surface mount design make them ideal for embedding in numerous applications. Lead frame versions are also offered. Units with an integrated photo IC have improved anti-noise characteristics.
Typical applications include:
- Audio Visual devices such as audio amplifiers, TVs, VCRs, and CD/DVD/MD players
- Multimedia equipment
- Home appliances such as air conditioners, fans, and lighting products
- CATV set top boxes
- Toys
- Any equipment with a wireless remote control
IR sensors have numerous applications in several market segments. A brief summary of markets and applications includes:
- Security – movement/motion detection, fire alarms/smoke detectors
- Industrial (including automotive) - measurement, counters, motor encoders
- Medical - blood/oxygen/temperature measurement
- Consumer - TVs/STBs, proximity sensors, cell phones, tilt sensors, ATMs/kiosks, and cameras
- Computers - keyboards/mice
- Printers - paper/media/door detection
- Game and Toys - remote control modules
As a wireless technology, IR has advantages and disadvantages when compared to RF and industrial, scientific, and medical (ISM) (902-928 MHz) band technologies. Advantages include:
- Higher security: beam directionality helps ensure that data isn’t detected or leaked to nearby devices as it’s transmitted
- High noise immunity: not as susceptible to signal interference from other devices
- Few international regulatory constraints
- Relatively low power requirements: ideal for laptops, cell phones, and personal digital assistants
- Simple design implementation
- Line of sight: transmitters and receivers must be almost directly aligned
- Blocked by common materials: people, walls, plants, and other objects can block transmission
- Short range: performance drops off with longer distances
- Light and weather sensitive: direct sunlight, rain, fog, dust, and pollution can affect transmission
- Speed: data rate transmission is lower than typical wired and RF transmission
ROHM Semiconductor IR solutions
ROHM Semiconductor offers several products to address each type of IR device technology. A few key products demonstrate a broad range of capabilities with a special focus on packaging.
IR emitters
ROHM Semiconductor IR optical sensor technology covers infrared light emitting diodes (LEDs). Several products are available in both surface mount (SMD) and through-hole (THD) configurations. Breakthrough IR wavelength emitter technology has resulted in the development of IR emitters that operate near 850 nm. As shown in Figure 6, phototransistors have a wide bandwidth but with a peak sensitivity at around 800 nm. The 850 nm level is much closer to this peak sensitivity (compared with conventional emitters that operate close to 950 nm), resulting in higher output efficiency and an energy savings of 66percent.
The new SIM-040ST demonstrates an improved peak wavelength (870 nm) and high IR power output (maximum of 100 mW/sr) in a 1.6 x 2.25 x 3.1 mm SMD package. The SIM-030ST, with similar performance, is offered in an even thinner (0.9 mm) and smaller (2.3 x 1.95 mm) form factor.
Figure 6: Unlike conventional IR emitters that operate near 950 nm, the 850 nm operation of ROHM Semiconductor’s IR wavelength emitter technology is much closer to the wavelength of phototransistors resulting in reduced energy losses.
IR phototransistors/sensors
ROHM Semiconductor IR phototransistors feature high gain and high collector current in a variety of packaging options. For example, the SCM-014TB is a top-view molded type with lens designed for automatic mounting and SMD reflow assembly, while the SML-810TB is a molded type lens design compatible with reverse mounting. The RPM-012PB is a high sensitivity, side-view sensor offered in an ultra-small 2 x 3 x 2 mm surface mount package featuring an ambient light filter, making it an ideal match with the SIM-012SB photoemitter.
Photointerrupters
ROHM Semiconductor offers photointerrupters in both transmission and reflective type designs. Utilization of double-mold construction (a primary mold with the lens followed by a secondary mold, see Figure 8) and 850 nm IR wavelength emitter technology result in high sensitivity, improved signal accuracy, and the highest collector output current in the industry.
Figure 7: Double-mold construction contributes to increased output in the RPI-2501 and other ROHM Semiconductor optical sensors.
The RPI-151 is a two-phase photointerrupter integrating two sensors in a single package. In addition to increased space savings, it can detect both the speed and direction of a motor with greater accuracy than conventional photo-optical solutions utilizing two separate sensors.
Figure 8: RPI-151 can detect both the spin speed and spin direction of a motor.
Reflective type sensors are offered in both through-hole and SMD package types and have a focal length (sensing reflection distance) of 3-6 mm. The main differentiating feature is the peak emitting wavelength - the RPR-220 features a wavelength of 940 nm, while the RPR-220UC30N and RPR-220PC30N are 950 nm and 470 nm, respectively.
Tilt sensors
Optimized for digital camera applications, the RPI-1040 is an optical surface mount 4-way detection sensor consisting of an IR LED and two phototransistors (see Figure 9). The 3.1 x 3.1 x 0.8 mm package - the thinnest in the industry - includes a novel light shield that ensures silent operation, avoiding noise frequently exhibited by other designs during rotation. In addition, the tilt sensor is not susceptible to vibration or external energy (RF, magnetic) fields. Ideal applications include orientation/fall/shock detection and image rotation.
IrDA communication modules
ROHM Semiconductor’s IrDA communication modules are among the smallest in the industry. Offered for SIR, MIR and FIR data rates, these units feature ultra-low power consumption. Some models offer adjustable LED current.
Figure 10: RPM871 IrDA communication module.
For example, the RPM871 is a micro infrared module based on the IrDA1.2 (Low Power) standard. This SIR-compliant product can operate at distances up to 60 cm and includes an infrared LED, PIN photodiode, and LSI circuitry in an ultra-compact, 8-pin package. In addition to low power consumption (73 µA typ.), the module features a power down function that reduces current consumption to 0.01 µA during standby.
Figure 11: Input noise capacity range vs noise frequency.
Remote control receiver modules
ROHM Semiconductor offers remote control receiver modules integrating two receivers in an ultra-compact surface mount design. Also available are 3 V and 5 V lead frame products featuring excellent anti-noise characteristics, as well as surface mount side and top view types.
Figure 12: RPM5540 remote control receiver module.
For example, the RPM5540 series of ultra-compact (3 x 8 x 2 mm) surface mount remote control receiver modules is available in both top view (H12) and side view (H14) configurations and is a sixteenth the size of conventional products. In addition, the dual-receiver design utilizes a 40 kHz carrier frequency, operates from a 5 V supply, and features a current consumption of only 0.95 mA (typ).
Conclusion
To address the increasingly broad range of IR applications, ROHM Semiconductor has established an extensive portfolio of IR sensor and remote control products that combine the latest IR technologies with unique ultra-compact packaging.
In addition, 40 years of IR sensor support and ongoing advancements in the fields of LEDs and sensors allow ROHM to meet current and future customer requirements. The wide product lineup includes both integrated as well as discrete solutions for standard and custom applications.
免责声明:各个作者和/或论坛参与者在本网站发表的观点、看法和意见不代表 DigiKey 的观点、看法和意见,也不代表 DigiKey 官方政策。