Maker.io main logo

Things to Consider When Designing With the KEMET SS-430 Sensor Module

2019-09-05 | By Dany Haikin

License: None

Recently KEMET released the series of their proximity (sometimes called motion) sensors modules:

sensors_1

All these modules are based on the proximity sensor chip PL-N823-01 (DKE p/n 399-17913-1-ND) which is Pyroelectric Infrared Sensor (aka PIR - Passive Infrared or IR motion sensors) and exists in the market for some time already. The sensor is based on Tokin (a vendor acquired by KEMET in 2017) patent technology that does not require the lens for operation up to 2m and can sense up to 20cm with resin or glass without a hole for a sensor. Using the lens as an option will increase the sensing distance up to 5 meters.

The sensor chip PL-N823-01 outputs analog voltage that should be amplified and connected to a MCU’s A/D for filtering and processing and fits the high volume or price sensitive applications and involves some design activity from the customer side.

The sensor modules mentioned above, have all the necessary circuitry built-in in the module, they are still rather small – about a dime size (Figure 1). The exact dimensions are shown in a module data sheet on https://content.kemet.com/datasheets/KEM_SE0208_SS.pdf

modules_2

Figure 1

I decided to test the sensor module SS-430 (without the lens).

The sensor modules SS-430 (and SS-430-N/W/BK with the lens) have just 3 pins to be used as per below table.

pins_3

The module has a JST connector on a Component mounted side of the module, JST p/n is SM05B-SRSS-TB(LF)(SN) (DK p/n 455-1805-1-ND). The product page of this connector on Digi-Key website, provides the information of the mating cables that can be used in "Associated Product" section. I used the blue cable made by Kemet with the open edges on the second side of the cable.

Component_4

The basic platform which was used to host the sensor, provide the necessary voltage and evaluate the sensor performance is Espressif IoT evaluation board ESP32-DEVKITC-32D-F (DK p/n 1965-1003-ND) powered through the USB cable.

board_5

Vin and GND pins of the sensor module are connected to 5v and GND in the ESP32 board respectively. Vout pin is connected to I/O pin 16 in the ESP32 board a will trigger the LED anode, connected to I/O pin 17 to turn ON/OFF the LED to better illustrate sensor operation.

operation_6

Figure 2

And finally I used Analog Devices Active Learning Module - ADALM2000 (DK p/n ADALM2000-ND) and PC resident software interface Scopy. This ADALM2000 is great low cost All-In-One lab tool suitable Students, hobbyists and self-Learners and is good for debugging the designs with low speed signals like in our case. https://media.digikey.com/pdf/Data Sheets/Analog Devices PDFs/ADALM2000_Web.pdf

device_7

First, I had to understand the sensor output behavior.

SS-430 Data Sheet shows that the output (Vout) of the sensor is 3v, one 200msec width pulse on detection after the stabilization period of 30 sec.

Sheet_8

This specification is not precise. Two important questions can be asked:

1. What happens when the object leaves the detection range?

2. What happens on non-movement or quick movements of the heat source inside the detection area?

I had made the following experiments to address these questions:

1. The sensor is used without any resin

2. The sensor is used with glass resin

1. The sensor is used without any resin

Before that need to take into account the following limitations of PIR technology. By definition of the Pyroelectric Infrared sensor, the sensor detects a heat source if there is more than 4℃ temperature difference from ambient temperature. However, because of the nature of the PIR sensor, it can detect the heat source regardless whether it is in the detection area, when the sensor is exposed to the following events or conditions:

Indirect and direct sun light, incandescent lamp, strong light beam, air flow from the air conditioner or chiller, frequent ambient temperature changes, strong electromagnetic fields, and strong vibrations, etc., etc.

All PIR sensors manufacturers mention some or all of above limitations in the “Cautions for Use” at the end of the Data Sheet.

Based on above “Cautions for Use”, looks like that KEMET SS-430 module is very sensitive to be tested in a office/lab standard environment on the table as the output is sending the pulses all the time even if the object is not in detection area as shown in Figure 3.

pulses_9

Figure 3

I assume that in order to test the sensor’s functionality for 1 – 2m range without a resin or glass, the sensor should be used in dark environment or properly housed to prevent the extenal distubances as listed above.

2. The sensor is used with a glass resin

In this environment, the sensor is “less sensitive” and can be tested in the standard lab during a day time. The detecting range will be several santimeters but it is enough for testing purposes. So I put a glass cup on the sensor. The bottom of the glass is rather thick, so only actually putting the hand on it causes the sensor to function. In real application using a thinner glass will increase the distance to specified 10-20 cm.

glass_10

glass2_11

The test environment was set up as following:

1. The sensor is connected to Espressif IoT evaluation board ESP32-DEVKITC as described in Figure 2.

2. Analog Devices ADALM2000 is used in oscilloscope mode and the orange channel 1 (out of 2 available) is connected to Vout pin of the sensor SS-430 (via I/O pin 16 in the ESP32 board).

3. The trigger of the scope is set for the rising edge of this channel 1 (Vout) waiting for the sensor to output the pulse.

4. The hand is touching the bottom of the glass and is removed with different time periods between touching and removing.

After many trials of touching and removing the hand from the bottom of the glass, the following were observed:

1. The output voltage is stable on zero volts if the hand does not touch the glass.

2. The sensor outputs the pulse/pulses both on detection of the heat source (the hand) and also when the heat source (the hand) leaves the detection range.

3. One or Two pulses signals are outputted from the sensor on both detection and leaving the detection range, depending on how fast the hand is moving. The distance between the multiple pulses is not constant, but they are close to each other. Figures 4, 5, 6 show the scope screen for this behavior. The first pulse/pulses are on touching the glass, the next series of the pulses are on removing the hand.

4. The sensor outputs One or Two pulses on detection and does not output any additional pulses as long as the heat source (the hand) is in detection range.

5. The output signals are 200 msec width as specified and are rather clean.

output_12

Figure 4

output2_13

Figure 5

output3_14

Figure 6

To illustrate the sensor behavior, I added a LED as shown in Figure 2. I decided to use Atmosphere IoT Studio which is the simplest and fastest way to create one sequential pulse between touching the glass and removing the hand from the glass to turn ON/OFF the LED without writing any code. It is not the most sophisticated way, but serves right the illustration purpose.

The falling edge of the sensor output pulse on I/O pin 16, triggers the counter, which counts 2 pulses as modulo 2 counter and on reset toggles the I/O pin 17 – turning the LED ON/OFF as shown on Figure 7.

ESP32_15

Figure 7

Figure 8 shows the output of the sensor (orange channel) with 2 pulses in touch-remove-touch sequence and purple channel shows the pulse generated by DK IoT studio that is driving the LED.

touch_16

Figure 8

The video 1 illustrates touching the glass that triggers the scope (the trigger of the scope is set for the rising edge of the channel 1 (Vout) waiting for the sensor to output the pulse) and turning the LED ON in parallel and then removing the hand from the glass is triggering the scope again and is turning the LED OFF.

The video 2 shows the sequence of 3 times touching/removing the hand from the glass that turns ON/OFF the LED. This video demonstrates that there are no additional pulses outputted from the sensor while the heat object is inside the detection range (the hand is on the glass).

To summarize:

1. The sensor SS-430 is very small and low profile module that well fits space critical applications and products where the sensor should be Inconspicuous.

2. The module can be operated without the lens.

3. To use the sensor without the resin or glass requires mechanical housing design to eliminate the environmental conditions that affect the sensor behavior.

4. The sensor can output One or Two pulses both on detecting the heat object and when the heat object passes away from the detection range.

The conclusion

To create a robust design that deals with multiple pulses output and creates the ON/OFF switch to drive another circuitry on detection, the use of a low cost MCU or Programmable Logic is needed to build a pulse-count circuit that counts the pulse/pulses appearance within 2-3 seconds time slot. That delay is tolerable by many applications using PIR proximity sensors. This will make KEMET sensor module SS-430 a real “Plug&Sense” module.

制造商零件编号 PL-N823-01
PYROELECTRIC SENSORS
KEMET
制造商零件编号 SS-430
PYRO SENSOR MODULE 60DEG 2M DIST
KEMET
制造商零件编号 SS-430L-BK
PYRO SENSOR MODULE 37DEG(H) 28DE
KEMET
制造商零件编号 SS-430L-N
PYRO SENSOR MODULE 37DEG(H) 28DE
KEMET
制造商零件编号 SS-430L-W
PYRO SENSOR MODULE 37DEG(H) 28DE
KEMET
制造商零件编号 ESP32-DEVKITC-32D-F
EVAL BOARD FOR ESP-WROOM-32
Espressif Systems
Add all DigiKey Parts to Cart
TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum