制造商零件编号 3093
CRICKIT CIRCUIT PLAYGROUND EXP
Adafruit Industries LLC
License: See Original Project Programmers Circuit Playground Adafruit Feather micro:bit
Courtesy of Adafruit
Guide by Anne Barela
Overview
Performing a search on robots of the past, most robots look unlit. Maybe some light for the eyes and not much else. Fortunately, anyone working with Adafruit Crickit, the Creative Robot and Interactive Construction KIT, can light their projects easily. There are numerous ways to light up your Crickit projects in only a couple of minutes.
This guide will show you how to use the NeoPixels on the Crickit and additional NeoPixels connected to the Crickit NeoPixel header. The code will be shown both in Microsoft MakeCode and in CircuitPython to allow you to integrate lights into your project quickly.
Whether you are looking for bling or serious environmental lighting, this is your starting point.
Different Types of Crickit Boards
There are several models of Crickit:
This guide will discuss NeoPixel connections in general for all boards and point out if anything is specific to a particular type of Crickit.
Parts List
Setting Up Your Programming Environment
If you are using Microsoft MakeCode or CircuitPython, you'll need to do a couple of basic things to set things up.
For MakeCode
In Makecode, the editor is located at https://makecode.adafruit.com/
You will need to add the Crickit extensions. The Crickit Guide has the MakeCode information page to install this extension.
For CircuitPython
See this guide page from Introducing Adafruit Crickit on setting up your CircuitPython environment.
Adafruit suggests using the Mu editor to edit your code and have an interactive REPL in CircuitPython. You can learn about Mu and installation in this tutorial.
Using the Crickit NeoPixel Terminal Block
All Adafruit NeoPixel products have three main pins:
At the end of the NeoPixels or on the same board for a ring is a Data Out (DOUT) pin to connect to another NeoPixel product Data In pin if needed.
Crickit has a NeoPixel terminal block as shown at left. It works perfectly for NeoPixel strip connections.
Check carefully for the wire colors and wire ordering as they may vary from product to product. The markings on the products are always consistent so check those strips, rings, etc. for the pin names.
The examples in this guide will use a strip of NeoPixels. You are free to mix in strips, rings, etc. If you plan to use more than 100 NeoPixels in total, please read the page "You Want Even More NeoPixels?" to get a feel for using a large number of pixels.
Note that you should not mix NeoPixels and Adafruit Dotstar products as they use separate types of wiring and software.
Differences Between Crickit Boards
This output is slightly different depending on what kind of Crickit you have:
MakeCode
MakeCode is for CircuitPlayground Express Crickit and micro:bit Crickit - it does not support Feathers at this time!
MakeCode
MakeCode has a large variety of code blocks which take advantage of the things you can do with NeoPixels. But in general, THIS ONLY WORKS FOR THE CIRCUIT PLAYGROUND CRICKIT and Crickit for micro:bit. The Feather Crickit NeoPixels are connected to the onboard seesaw chip so use in MakeCode isn't currently supported.
Circuit Playground Express + Crickit with MakeCode
In the LIGHT block group, there is a special subgroup that pops below LIGHT when LIGHT is pushed called ... NEOPIXEL. This provides a huge number of blocks to work with NeoPixels that are not on your Crickit or the microcontroller on Crickit like a Circuit Playground Express.
For Circuit Playground Express, the Crickit NeoPixel Terminal is connected to CPX Pin A1. When you use the MakeCode NeoPixel blocks to manipulate your externally connected NeoPixels, you need to use the NEOPIXEL subgroup block labeled set strip to create strip.
For the code below, I have connected a 30 NeoPixel strip to the Crickit NeoPixel terminal block. When the program starts, the on start code up the variable named strip to refer to a NeoPixel strip connected to A1 (which all Crickit strips are connected to) with 30 NeoPixels on it (You have to click the + on the block to specify the pin A1 and add the number of NeoPixels.
Then the program shows the rainbow animation on the strip forever. You can change the animation type or do lots of other things on your strip. It's that easy!
Crickit FeatherWing
There currently is no MakeCode support for the FeatherWing Crickit! Please use Arduino or CircuitPython for your Feather+Crickit needs
micro:bit and Crickit
For micro:bit, there is a small sun icon on Pin P16 on Crickit to help you remember that is the pin connected for NeoPixels.
You need to add the NeoPixels extension to MakeCode for micro:bit for NeoPixel control. Click the Advanced button then Add Package. Select the Adafruit NeoPixels extension. You will now have a new code block group called Neopixel which has the blocks you want to control the NeoPixel strip.
The code below does what the above code does for CPX - creates a strip of 30 NeoPixels connected to Pin 16 and then displays a rainbow animation forever.
Open this example in MakeCode for micro:bit
CircuitPython
The sample code below is a tiny bit different depending if you have a Crickit for Circuit Playground Express or Crickit FeatherWing.
Both have some functions to make some colorful animations. Feel free to change the lighting to suit your project.
To pick your own color values, see http://www.color-hex.com/ to find your favorite red, green, and blue to place in your code!
Crickit with Circuit Playground Express
The NeoPixel terminal block is controlled by the Circuit Playground Express pad A1. The pad A1 definition is obtained by import board. Then the NeoPixel routine is from import neopixel.
Various animations are provided by defined functions wheel, color_chase and rainbow_cycle. Various solid colors are then defined, you are free to use whichever colors you wish.
You can define a new color variable as a Python tuple with three values for red, green, blue, for example WHITE = (255, 255, 255).
# Drive NeoPixels on the NeoPixels Block on Crickit for
# Circuit Playground Express
import time
import neopixel
import board
num_pixels = 30 # Number of pixels driven from Crickit NeoPixel terminal
# The following line sets up a NeoPixel strip on Crickit CPX pin A1
pixels = neopixel.NeoPixel(board.A1, num_pixels, brightness=0.3,
auto_write=False)
def wheel(pos):
# Input a value 0 to 255 to get a color value.
# The colours are a transition r - g - b - back to r.
if pos < 0 or pos > 255:
return (0, 0, 0)
if pos < 85:
return (255 - pos * 3, pos * 3, 0)
if pos < 170:
pos -= 85
return (0, 255 - pos * 3, pos * 3)
pos -= 170
return (pos * 3, 0, 255 - pos * 3)
def color_chase(color, wait):
for i in range(num_pixels):
pixels[i] = color
time.sleep(wait)
pixels.show()
time.sleep(0.5)
def rainbow_cycle(wait):
for j in range(255):
for i in range(num_pixels):
rc_index = (i * 256 // num_pixels) + j
pixels[i] = wheel(rc_index & 255)
pixels.show()
time.sleep(wait)
RED = (255, 0, 0)
YELLOW = (255, 150, 0)
GREEN = (0, 255, 0)
CYAN = (0, 255, 255)
BLUE = (0, 0, 255)
PURPLE = (180, 0, 255)
while True:
print("fill")
pixels.fill(RED)
pixels.show()
# Increase or decrease to change the speed of the solid color change.
time.sleep(1)
pixels.fill(GREEN)
pixels.show()
time.sleep(1)
pixels.fill(BLUE)
pixels.show()
time.sleep(1)
print("chase")
color_chase(RED, 0.1) # Increase the number to slow down the color chase
color_chase(YELLOW, 0.1)
color_chase(GREEN, 0.1)
color_chase(CYAN, 0.1)
color_chase(BLUE, 0.1)
color_chase(PURPLE, 0.1)
print("rainbow")
rainbow_cycle(0) # Increase the number to slow down the rainbow
Crickit FeatherWing
The NeoPixel block signal wire is connected to the Crickit Seesaw control chip pin #20. The following code sets up an external 30 NeoPixel strip.
# Drive NeoPixels on the NeoPixels Block on Crickit FeatherWing
import time
from adafruit_crickit import crickit
from adafruit_seesaw.neopixel import NeoPixel
num_pixels = 30 # Number of pixels driven from Crickit NeoPixel terminal
# The following line sets up a NeoPixel strip on Seesaw pin 20 for Feather
pixels = NeoPixel(crickit.seesaw, 20, num_pixels)
def wheel(pos):
# Input a value 0 to 255 to get a color value.
# The colours are a transition r - g - b - back to r.
if pos < 0 or pos > 255:
return (0, 0, 0)
if pos < 85:
return (255 - pos * 3, pos * 3, 0)
if pos < 170:
pos -= 85
return (0, 255 - pos * 3, pos * 3)
pos -= 170
return (pos * 3, 0, 255 - pos * 3)
def color_chase(color, wait):
for i in range(num_pixels):
pixels[i] = color
time.sleep(wait)
pixels.show()
time.sleep(0.5)
def rainbow_cycle(wait):
for j in range(255):
for i in range(num_pixels):
rc_index = (i * 256 // num_pixels) + j
pixels[i] = wheel(rc_index & 255)
pixels.show()
time.sleep(wait)
RED = (255, 0, 0)
YELLOW = (255, 150, 0)
GREEN = (0, 255, 0)
CYAN = (0, 255, 255)
BLUE = (0, 0, 255)
PURPLE = (180, 0, 255)
while True:
print("fill")
pixels.fill(RED)
pixels.show()
# Increase or decrease to change the speed of the solid color change.
time.sleep(1)
pixels.fill(GREEN)
pixels.show()
time.sleep(1)
pixels.fill(BLUE)
pixels.show()
time.sleep(1)
print("chase")
color_chase(RED, 0.1) # Increase the number to slow down the color chase
color_chase(YELLOW, 0.1)
color_chase(GREEN, 0.1)
color_chase(CYAN, 0.1)
color_chase(BLUE, 0.1)
color_chase(PURPLE, 0.1)
print("rainbow")
rainbow_cycle(0) # Increase the number to slow down the rainbow
Using Circuit Playground Express NeoPixels
Using the on-Board Circuit Playground Express NeoPixels
The Circuit Playground Express has ten Neopixels of its own that can be programmed independently from the Crickit single NeoPixel and Crickit NeoPixel terminal block connection.
MakeCode
For the Crickit NeoPixels we used the NEOPIXEL subgroup of the LIGHT block group in MakeCode. For the Circuit Playground Express, you use the blocks directly in the LIGHT block group, not the NEOPIXELS subblock blocks.
Below are two example programs (use one or another). The first just sets all the Circuit Playground Express LEDs to green. The second shows a rainbow animation for 5 seconds (= 5000 milliseconds), then shows a sparkle animation for another 5 seconds then loops back.
More on MakeCode and the Circuit Playground Express on the Introduction to Circuit Playground Express tutorial.
CircuitPython
It takes a bit more code to do NeoPixels in CircuitPython. The easiest way is to use the adafruit_circuitplayground.express library which sets everything up nicely. But the CPX library, as it's called, is large and when added to the Crickit support library adafruit_crickit, it does not leave a great amount of room for user programs.
The same effects in the CPX library may be done with the neopixel library, it is just coded a bit differently.
The code below shows opening up the NeoPixels on-board and performing some red and blue color animation which you are free to change as you wish. The code for the strips to change color in previous examples will work here also with appropriate variable name changes for the NeoPixel object opened.
# Use the 10 NeoPixels on Circuit Playground Express via the
# Adafruit neopixel library
import time
import neopixel
import board
# Set up the 10 Circuit Playground Express NeoPixels half bright
CPX_pixels = neopixel.NeoPixel(board.NEOPIXEL, 10, brightness=0.5)
# slowly power up via blue color
for i in range(50):
CPX_pixels.fill((0, 0, i))
time.sleep(0.05)
# blast off!
CPX_pixels.fill((255, 0, 0))
while True:
# pulse effect
for i in range(255, 0, -5):
CPX_pixels.fill((i, 0, 0))
for i in range(0, 255, 5):
CPX_pixels.fill((i, 0, 0))
Using the Crickit Single LED
It isn't recommended that you use the Crickit NeoPixel LED because we use it to report when the battery is low! However, if you're curious, here's how to do it
The On-board Crickit NeoPixel is great for providing status information to the user. It can also function as a light to help you find your bot in the dark.
This page will quickly show you how to use this NeoPixel.
MakeCode
You can use the three special NeoPixel blocks in the CRICKIT block group extension to change the single NeoPixel on-board Crickit. They work just like the NeoPixel blocks under the LIGHT block group but just for the one Crickit pixel.
You can independently set a color for the NeoPixel, turn it off, or set the brightness.
CircuitPython
The internal NeoPixel is on the Crickit's seesaw controller, pin #27. In addition to importing the adafruit_crickit library you'll need the adafruit_seesaw.neopixel library also.
# Using Crickit's onboard NeoPixel
# See http://www.color-hex.com/ for more colors and find your fav!
from adafruit_crickit import crickit
from adafruit_seesaw.neopixel import NeoPixel
crickit_status_pixel = NeoPixel(crickit.seesaw, 27, 1) # one NeoPixel pin 27
# Fill them with our favorite color "#0099FF light blue" -> 0x0099FF
crickit_status_pixel.fill(0x0099FF)
while True:
pass
The fill function will set the pixel to the hex code for red, green, and blue for the pixel. To turn the NeoPixel off, use a value of zero, such as crickit_status_pixel.fill(0x000000).
You Want Even More NeoPixels?
NeoPixels in all sorts of shapes (credit: Adafruit)
Memory
The main limitation on use of NeoPixels on many microcontrollers is memory. The microcontroller, in general, has to reserve at least three bytes for the red, green, and blue pixel values. The more pixels to control, the more memory is used.
M0 based products like Circuit Playground Express and Feather M0 Express can usually drive about 100 pixels easily. With the Feather M4 Express, this is increased. The maximum will have to be something you test as with code, the amount of free RAM varies. 300 pixels may be possible on Feather M4.
If you plan to drive a large number of pixels, like for a whole room or art project, look at the full range Adafruit Products and guides. And catch us on the Adafruit forums under Glowy Things and on the Adafruit Discord channel. Folks can guide you to something if it is larger than can be accommodated with this introductory guide.
Power and Current
Crickit is designed to handle a decent amount of power (current) to your NeoPixel projects. Power = current x voltage, so with a constant 5 volts, power increases proportionally to current needs.
You will need to get an appropriate power supply to handle the peak (maximum) current you plan to draw in your project.
For a static (non-mobile) project, Adafruit recommends the 5V 2 Amp supply for Crickit use.
If you plan on lots of motors and lots of NeoPixels, you can use a power supply up to 4 amps. If you were to use 100 LEDs on full white, you might draw 4 amps according to Ladyada. If you do not run the LEDs all at full brightness and color, your project will use less current and save your eyeballs from the bright light.
If you don't run your NeoPixels full bright, say 30%, you may get up to 300 pixels running if you have enough memory free on the microcontroller you are using on your Crickit.
If you are running into limitations on the Crickit current use, you may have to look at a more sophisticated design. More often than not you'll run out of memory sooner than current capacity for the LEDs.