Make a Pi Trash Classifier with Machine Learning and Lobe
2020-12-01 | By Adafruit Industries
License: See Original Project
Courtesy of Adafruit
Guide by Jen Fox
Overview
The Trash Classifier project, affectionately known as "Where does it go?!", is designed to make throwing things away faster and more reliable.
Lobe: a beginner-friendly program to make custom ML models!
This project uses a Machine Learning (ML) model trained in Lobe, a beginner-friendly (no code!) ML model builder, to identify whether an object goes in the garbage, recycling, compost, or hazardous waste. The ML model is loaded onto a Raspberry Pi computer to make it usable wherever you might find rubbish bins!
This tutorial walks you how to create your own Trash Classifier project on a Raspberry Pi from a Lobe TensorFlow Lite model in Python3.
Difficulty: Beginner++ (some knowledge w/ circuits and coding are helpful)
Read Time: 10 min
Build Time: 60 - 90 min
Tools and Materials
Hardware
- Raspberry Pi 4 Model B - 2 GB RAM
- Raspberry Pi Camera Board v2 - 8 Megapixels
- Official Raspberry Pi Power Supply 5.1V 3A with USB C
- SD/MicroSD Memory Card (8 GB SDHC)
- Half-size breadboard
- 1 x Pushbutton
- 1 x LEDs
- 1 x 220 Ohm Resistors
- 1 x Jumper wires
If you choose to solder:
- 1 JST connector, female end only
- 2 M-to-F jumper wires
- 10 F-to-F jumper wires
- Heat Shrink Tubing
- PCB - Half Perma Proto Board
Enclosure
- Project case (e.g. cardboard, wood, or plastic box, approx. 6" x 5" x 4")
- 0.5" x 0.5" (2cm x 2cm) clear plastic square
- E.g. from a plastic food container lid
- Velcro
Tools
- Wire cutters
- Soldering iron
- Helping Hands (optional)
- Precision knife (e.g. exacto knife) and cutting mat
- Hot melt tool (or other non-conductive glue -- epoxy works great but is permanent)
Software (PC-side)
- Lobe
- WinSCP (or other SSH file transfer method, can use CyberDuck for Mac)
- Terminal
- Remote Desktop Connection or RealVNC
Before Starting
This project assumes you're starting with a fully set-up Raspberry Pi in a headless configuration. Here's a beginner-friendly guide on how to do this.
It also helps to have some knowledge of the following:
1. Familiarity with the Raspberry Pi
2. Reading and editing Python code (you won't need to write a program from scratch, just edit.)
3. Reading Fritzing wiring diagrams
4. Using a breadboard
Find out where your trash goes
Each city across the US (and I would assume the globe) has its own garbage/recycling/compost/etc. collection system. This means that to make an accurate trash classifier, we'll need to 1) build a custom ML model (we'll cover this in the next step -- no code!) and 2) know where each piece of trash goes.
Since I didn't always know the proper bin for each item I used to train my model, I used the Seattle Utilities flyer shown above, and also this handy "Where does it go?" lookup tool for the city of Seattle! Check out what resources are available in your city you by looking up your city's garbage collection utility and perusing its website.
Create a Custom ML model in Lobe
Lobe is an easy-to-use tool that has everything you need to bring your machine learning ideas to life. Show it examples of what you want it to do, and it automatically trains a custom machine learning model that can be exported for edge devices and apps. It doesn’t require any experience to get started. You can train on your own computer for free!
Here's a quick overview on how to use Lobe:
1. Open the Lobe program and create a new project.
2. Take or import photos and label them into appropriate categories. We'll need these labels later on in the software part of the project.
There are two ways to import photos:
1. Take photos of items directly from your computer webcam, or
2. Import existing photos from your computer (via single photo or folder/dataset upload.)
- Keep in mind that the photo folder name will be used as the category label name, so make sure it matches any existing labels!
Aside: I ended up using both methods, since the more photos you have, the more accurate your model is.
3. Use the "Play" feature to test the model accuracy. Change distances, lighting, hand positions, etc. to identify where the model is and is not accurate. Add more photos as necessary.
4. When you're ready, export your Lobe ML model in a TensorFlow (TF) Lite format.
Tips:
- Before importing photos, make a list of all the categories you'll need and how you want to label them (e.g. "garbage," "recycle," "compost," etc.)
- Note: Use the same labels as shown in "Lobe Model Labels" photo above to reduce the amount of code you need to change.
- Include a category for "not trash" that has photos of whatever else might be in the photo (e.g. your hands and arms, the background, etc.)
- If possible, take photos from the Pi Camera and import into Lobe. This will greatly improve the accuracy of your model!
- Need more photos? Check out open-source datasets on Kaggle, including this garbage classification image set!
- Need more help? Connect with the Lobe Community on Reddit!
Build it: Hardware
1. Carefully connect the Pi Camera to Pi (visit the Pi Foundation getting started guide for more information.)
2. Follow the wiring diagram to connect the pushbutton and LEDs to the Pi GPIO pins.
- Pushbutton: Connect one leg of the pushbutton to GPIO pin 2. Connect the other, via a resistor, to a GPIO GND pin.
- Yellow LED: Connect the positive (longer) leg to GPIO pin 17. Connect the other leg, via a resistor, to a GPIO GND pin.
- Blue LED: Connect the positive leg to GPIO pin 27. Connect the other leg, via a resistor, to a GPIO GND pin.
- Green LED: Connect the positive leg to GPIO pin 22. Connect the other leg, via a resistor, to a GPIO GND pin.
- Red LED: Connect the positive leg to GPIO pin 23. Connect the other leg, via a resistor, to a GPIO GND pin.
- White LED: Connect the positive leg to GPIO pin 24. Connect the other leg, via a resistor, to a GPIO GND pin.
3. It is recommended to test your circuit on a breadboard and run the program before soldering or making any of the connections permanent. To do this, we'll need to write and upload our software program, so let's go to the next step!
Code it: Software
1. On your PC, open WinSCP and connect to your Pi. Create a Lobe folder in your Pi's home directory and create a model folder in that directory.
2. Drag the resulting Lobe TF folder contents onto the Pi. Make note of the file path: /home/pi/Lobe/model
3. On the Pi, open a terminal and download the lobe-python library for Python3 by running the following bash commands:
pip3 install setuptools
pip3 install tensorflow==1.13.1
pip3 install git+https://github.com/lobe/lobe-python
4. Download the Trash Classifier code (rpi_trash_classifier.py) from this repo onto the Pi (click the "Code" button as shown in Photo 1.)
- Prefer to copy/paste? Snag the code below!
- Prefer to download onto your computer? Download the repo/code onto your computer then transfer the Python code to the Pi via WinSCP (or your preferred remote file transfer program)
5. Once you've connected the hardware to the Pi's GPIO pins, read through the example code and update any file paths as needed:
- Line 29: filepath to the Lobe TF model
- Lines 47 and 83: filepath to captured images via Pi Camera
6. If necessary, update the model labels in the code to exactly match the labels in your Lobe model (including capitalization, punctuation, etc):
- Line 57: "garbage"
- Line 60: "recycle"
- Line 63: "compost"
- Line 66: "hazardous waste facility"
- Line 69: "not trash!"
Download: file
# ------------------------------------------------------------------------
# Trash Classifier ML Project
# Please review ReadMe for instructions on how to build and run the program
#
# (c) 2020 by Jen Fox, Microsoft
# MIT License
# --------------------------------------------------------------------------
#import Pi GPIO library button class
from gpiozero import Button, LED, PWMLED
from picamera import PiCamera
from time import sleep
from lobe import ImageModel
#Create input, output, and camera objects
button = Button(2)
yellow_led = LED(17) #garbage
blue_led = LED(27) #recycle
green_led = LED(22) #compost
red_led = LED(23) #hazardous waste facility
white_led = PWMLED(24) #Status light and retake photo
camera = PiCamera()
# Load Lobe TF model
# --> Change model file path as needed
model = ImageModel.load('/home/pi/Lobe/model')
# Take Photo
def take_photo():
# Quickly blink status light
white_led.blink(0.1,0.1)
sleep(2)
print("Pressed")
white_led.on()
# Start the camera preview
camera.start_preview(alpha=200)
# wait 2s or more for light adjustment
sleep(3)
# Optional image rotation for camera
# --> Change or comment out as needed
camera.rotation = 270
#Input image file path here
# --> Change image path as needed
camera.capture('/home/pi/Pictures/image.jpg')
#Stop camera
camera.stop_preview()
white_led.off()
sleep(1)
# Identify prediction and turn on appropriate LED
def led_select(label):
print(label)
if label == "garbage":
yellow_led.on()
sleep(5)
if label == "recycle":
blue_led.on()
sleep(5)
if label == "compost":
green_led.on()
sleep(5)
if label == "hazardous waste facility":
red_led.on()
sleep(5)
if label == "not trash!":
white_led.on()
sleep(5)
else:
yellow_led.off()
blue_led.off()
green_led.off()
red_led.off()
white_led.off()
# Main Function
while True:
if button.is_pressed:
take_photo()
# Run photo through Lobe TF model
result = model.predict_from_file('/home/pi/Pictures/image.jpg')
# --> Change image path
led_select(result.prediction)
else:
# Pulse status light
white_led.pulse(2,1)
sleep(1)
7. Run the program using Python3 in the terminal window:
python3 rpi_trash_classifier.py
Test it: Run the Program
Testing the program to ensure it works and correctly classifies recycling!
Program Overview
When you first run the program, it will take some time to load the TensorFlow library and the Lobe ML model. When the program is ready to capture an image, the status light (white LED) will pulse.
Once you've taken an image, the program will compare the image to the Lobe ML model and output the resulting prediction (line 83). The output determines which light is turned on: yellow (garbage), blue (recycle), green (compost), or red (hazardous waste.)
If none of the indicator LEDs turn on and the status LED returns to pulse mode, it means that the image captured was "not trash", in other words, retake the photo!
Capturing an Image
Press the pushbutton to capture an image. Note that you may need to hold the pushbutton for at least 1 second for the program to register the press. It is recommended to take some test images, then open them on the Desktop to better understand the camera view and frame.
To allow the user time to position the object and for camera light levels to adjust, it takes about 5s to fully capture an image. You may change these settings in the code (lines 35 and 41), but keep in mind the Pi Foundation recommends a minimum of 2s for light level adjustment.
Troubleshooting
The biggest challenge is ensuring that the captured image is what we expect, so take some time to review the images and compare expected results with indicator LED output. If necessary, you can pass in images to the Lobe ML model for direct inferencing and faster comparison.
A few things to note:
- The TensorFlow library will likely throw some warning messages -- this is typical for the version used in this sample code.
- The prediction labels must be exactly as written in the led_select() function, including capitalization, punctuation, and spacing. Be sure to change these if you have a different Lobe model.
- The Pi requires a steady power supply. The Pi's power light should be bright, solid red
- If one or more LEDs are not turning on when expected, check by forcing them on with the command:
red_led.on()
(Optional) Build it: Finalize the circuit
Finished LED connection
Now that we've tested and, if necessary, debugged, our project so that it works as expected, we're ready to solder our circuit!
Note: If you do not have a soldering iron, you may skip this step. One alternative is to coat the wire connections in hot glue (this option will allow you to fix/add/use things later, but is more likely to break), or use epoxy or a similar permanent glue (this option will be much more durable but you will not be able to use the circuit or potentially the Pi after doing this.)
Quick comment about my design choices:
- I opted for female jumper wires for the LEDs and Pi GPIO because they allow me to remove LEDs and swap colors or move them around if needed. You may skip these if you want to make connections permanent.
- Similarly, I chose a JST connector for the pushbutton.
Onward to building!
1. Cut each of the female jumper wires in half (yes, all of them!). Using wire strippers, remove about 1/4" (1/2cm) of the wire insulation.
2. For each of the LEDs, solder a 220Ω resistor to the negative (shorter) leg. A helping hands tool can help in holding things steady.
3. Cut a small piece, about 1" (2cm) of heat shrink tube and push over the LED and resistor junction. Make sure the other resistor leg is accessible, then heat up the shrink tube until it secures the joint.
4. Insert each LED into a pair of female jumper wires.
5. Label the jumper wires (e.g. with tape), then solder jumper wires onto your printed circuit board (PCB). WIth the perma Proto board, you can use the same locations you used in the breadboard setup.
6. Next, use a (cut) female jumper wire to connect each LED to its respective Pi GPIO pin. Solder and label a jumper wire so that the bare metal connects to the positive LED leg via the PCB.
Note: Where you solder this wire will depend on your PCB layout. You can also solder this wire directly to the positive LED jumper wire.
7. Solder a 220Ω resistor to the negative (black) end of the JST connector.
8. Solder the JST connector and resistor to the pushbutton.
9. Connect the M-to-F jumper wires between the pushbutton connector and the GPIO pins (reminder: black is GND.)
10. Coat connections PCB in hot glue or epoxy for a more secure connection.
Note: If you choose to use epoxy, you may not be able to use the Pi's GPIO pins for other projects in the future. If you're concerned about this, add in a GPIO ribbon cable and connect the jumper wires to that instead.
(Optional) Build it: Case
Create an enclosure for your Pi that will hold the camera, pushbutton, and LEDs in place while also protecting the Pi.
Design your own enclosure or follow our build instructions below for quickly prototyping a cardboard enclosure!
1. On the top of the small cardboard box, trace the locations for the pushbutton, status light, identifier lights, and the pi camera window.
• Note: Pi camera window should be about 3/4" x 1/2".
2. Using your precision knife, cut out the traces.
• Note: You may want to test the sizes as you go.
3. You can paint the box if you wish. Mount the pushbutton.
4. Cut out a rectangular "window" cover for the Pi Camera (Photo 4) and glue on the inside of the box.
5. Finally, cut out slot for the Pi power cable.
- Recommended to first install all electronics to locate the best place for the pi power cable slot.
Install and Deploy
That's it! You're ready to install and deploy your project! Place the enclosure above your trash bins, plug in the Pi, and run the program to get a faster, more reliable way of reducing our waste. Yay!