制造商零件编号 2163
SOLDERING IRON 50W 120V
Adafruit Industries LLC
License: See Original Project
Courtesy of Adafruit
Guide by Paul Beaudet
Overview
What's DDR?
Dance Dance Revolution or DDR for short is a rhythm game that is played with a directional pad made for feet. Coordination and rhythm is tested by watching on screen dance notes making steps to the keys of the beat. It's a simple step on up down left or right and sometimes even combinations of steps. DDR has been very popular in arcades and on game consoles. Now-a-days, however, the game can be enjoyed with a clone games like "Beats" for android, "Stepmania" for the desktop, or even FFR (flash flash revolution) online. This tutorial generally explains how to go about building a wireless game pad on the cheap to avoid buy expensive adapters or pads. Bluetooth control with Bluefruit EZ-Key honestly works so easily for that there is very little to explain about the controller beyond what is covered in the Bluefruit tutorial. No programing required! As opposed to using a HID emulating micro like the Arduino Leonardo which would require some small bits of code and a wire.
Materials
A number of different materials could be used in this project for the dance pad component. It’s all a tradeoff between reliability/quality, portability and cost. This tutorial prioritizes portability and cost. Using materials that might be found around the house or are affordable to get from the hardware store.
Cheapo method - As Shown
Quality approach- Recommended
Holding it all together
Duct tape, Foil tape (AKA actual metal duct tape not the plasticy gray stuff, although you need that too), hot glue, Velcro. More or less whatever it takes. In the following a lot of duct tape is use. There are likely more elegant ways to do it.
Controller
It is possible to easily do this with the Arduino Leonardo or Micro and some simple code for a wired set up but using OTG with android can sometimes be a hit or miss affair and wires are cumbersome. For a similar price, just get a Bluefruit EZ-Key! No programing required and its wireless! Most Bluetooth projects and products are a nightmare. Bluefruit is a dream.
The Bluefruit EZ-Key HID is recommended as it makes this project super simple. For this project the headers were soldered on and the EZ-Key was placed on a breadboard stuck to a 4 AA power supply. One might also decide to power their project with a Lipo battery and Charge Controller combo. Follow the EZ-Key tutorial for a better understanding of its pins and power requirements. The simplified dance pad only requires the use of 6 pins. Vin, Ground, and 0-3.
Pin cheat sheet for DDR
Tools and Prep
We'll start by making the dance pad itself, then add the Bluetooth part!
Tools
Design Note
A traditional dance pad has 10 buttons, but for the sake of simplicity and portability this design only incorporates the 4 most important buttons, UP, DOWN, LEFT, RIGHT. In Android with the "Beats" application which can be found in the Play Store, it is easy enough to touch the screen to select a song. Backing out of songs is for wusses, so that button can also be excluded. The other last 4 buttons are honestly redundant unless navigating through the console game menus.
Preparation
Cut the sign board into 8 (11"/ 28cm) squares. With sign board its useful to leave extra space and trim down to the cells. In a high-quality version, 4 rubber sheets and 4 Plexiglass sheets might be a good substitute.
Cut the foam into 16 small rectangles (about 1" x 2"), exact size depends on the type of foam used. Soft more, hard less, fairly soft foam is used in this pad. Hard or thick foam may make the pad difficult to use. Real pads use perforated sheets of thin (1/4") foam, this works well if thin foam sheets can be found. The redundant buttons on old pads provide good sheets. The directional key foam on store bought pads normally is the first thing to wear and lose resiliency. Making a faulty or unreliable pad. Another idea to separate the pad contacts might be short and wide springs given they are insulated from the contacts and fastened properly.
8 pieces of aluminum foil are needed to act as the pad contacts. About 70-90% of the square size is sufficient. In a higher quality version, it would be nice to use sheet metal. Drilling holes for the contact wires fishing them through and soldering in place. In this case contacts will be "secured" with foil tape. It works well enough, but for how long is another question.
No really, cut away from yourself. It's a good idea.
Assembly
Step 1
Connect the power supply and test the Bluefruit to be sure it pairs.
Step 2
Prepare vinyl top. As shown in previous illustrations the redundant portions are cut from an old dance pad. This could be substituted with a plus shaped cut out of vinyl or other sheet material with similar qualities. Duct tape could make a sheet like this given some level of desperation. In this affordable case the vinyl also doubles as 4 hinges to the portable box conversion.
Step 3
If still untouched, solder the headers on the Bluefruit and bread board it on to the power supply. Alternatively solder needed wire directly. This project used less than 6' of CAT 3, which is a 4-strained solid core wire. Whatever is on hand will work. Cut into two 3' pieces gives 8 lines. 4 for ground and 4 for the pins. Needless to say, keep track on the wire colors. The 4 ground wires are common, they can be soldered into one wire at one end and connected to one of the grounds on the Bluefruit. Both of the wires can be fished through the sign board cells in the bottom "up" pad. This brings the wires to the middle of the four button pads.
Step 4
Glue sheets of aluminum foil to sign board squares. Be sure to center and abut the best edge of the foil to one side. This side will face the inside of the pad. Where connections will be made to the foil.
Build Buttons
Step 5
Adhere the foam like in the picture, except slightly further apart. In hindsight the foam pieces in this up button were placed too close to the center making it more difficult to register a hot dance move.
Step 6 or 7
Depending on which way seems easier. The top pad can be glued to the foam completing the sandwich or the wires can be foil taped to the pads. Given patience for the sandwiches to be made they were done first in this project, but doing the connections first is also valid, particularly for one with big fingers.
Two buttons
Making connections
Foil tape will be used for this because of its conductive properties. Poke a pin hole in a half inch tear off, of tape after peeling. Push wire through this hole so that the bare wire gets stuck on the adhesive side and insulation is on the shiny side. Secure the insulation to the shiny side with another smaller piece of tape. Now stick that little electrode on the edge of one of the foil pads.
So long as all the pins go to a separate button this should come out right. It’s a simple circuit. Resistance is handled by a pull-up on the Bluefruit chip.
Test Connection
Break out the multimeter!
Along the way, test if the button works like... a button. When you press it, the metallic parts will touch, making a continuous connection.
Be sure the glue is set before pressing!!!!
We have a great tutorial on using multimeters, or just watch Collin's lab on multimeters in continuity mode.
Finishing touches
Glue the vinyl graphic on
Again, test it before wrapping things up for good. Wait for the glue to cool or dry.
Manage the wires
Probably should do it neater than this. Another piece of vinyl can be used to cover the bottom opening, just leave room for the "hinges" to move.
Add some Velcro straps
To convert into a box for portability
Done!
until you or your friend breaks it.