Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Product List
Following this decision tree, the engineer starts with the application temperature, which is quite simple to choose as there are only two ranges to choose from. Following the higher range of -55 to 125°C, the next item to consider is the capacitance stability or change rate. For a very stable capacitance, users will want to select the NPO option. In contrast, the X7R will be a viable option for those who are unconcerned with capacitance stability.
PTM Published on: 2011-11-09
PTM Updated on: 2018-08-31