Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
How to Select a Tripp Lite PDU Slide 15

Most mission-critical network devices feature redundant power supplies (each with its own power cord) that can connect to separate power sources. However, many other network devices do not have this redundant capability because they only have one power cord. Tripp Lite Automatic Transfer Switch (ATS) PDUs provide redundancy for these single-corded devices by allowing them to connect to two separate input power sources. Tripp Lite Automatic Transfer Switch  PDUs feature two input power cords and an automatic transfer switch (ATS). Network managers can plug the PDU's cords into two separate power sources. Depending on the desired level of power protection, the two sources can be two UPS systems, two generator-supported utility wall outlets, or one UPS system and one generator-supported utility wall outlet. When the primary input power source is normal, the PDU uses it to power connected equipment. If power fails or voltage drops below acceptable limits, a highly-reliable mechanism within the ATS automatically switches to the secondary input source to power connected equipment. These features allow managers to increase network availability by providing equipment with a redundant, backup source of power.

PTM Published on: 2015-03-23