Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Product List
The 15W DRB model can operate at full load at 70°C. The other power levels can deliver 50% output power at 70°C, derating linearly above 55°C. Below -10°C, the DRB models require output power derating for startup purposes only.
PTM Published on: 2014-01-20