In addition, TDK’s CKC Series has an optional soft termination benefit for crack mitigation purposes. The graph on this slide highlights the result of a tumbling test, which is conducted by “dropping” the board mounted capacitor from a height of 1 meter, 10,000 times, with an additional biased humidity test at the end. This facilitates the understanding of how board mounted capacitors react in situations where products are repeatedly dropped, such as mobile phones. As one can see, the soft termination array capacitor did not crack and also passed the biased humidity test after the tumbling cycles.