Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Reed Switch Magnet Interaction Slide 8

In this case, the magnet is centered over the central and strongest lobe. When the magnet moves downward and reaches the pull-in line the reed contacts will close. As the magnet is withdrawn vertically and upwards, the magnet will reach the dotted drop-out line. When this occurs the reed contacts will open. This represents a reed sensor cycle showing the sensing closure point and the sensing opening point. As long as the magnet is within the pull-in boundary (the solid lines) the contacts will remain closed. Once the magnet is withdrawn and outside the dotted drop-out lines the contacts will always be open. The center lobe is the strongest and will offer the greatest sensing distance when compared to the two side lobes.

PTM Published on: 2012-03-21