Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
auto-liquid-slide21

Generally in the cab of the vehicle the operating temperature is considerably better than the ‘under the hood’ environment but it still can range from -45°C to as high as 60°C. The braking operations not only activate the brake shoes through a hydraulics system, but the sensor sensing the brake pedal movement must turn on the brake lights and disengage the cruise control. In heavy traffic, sudden stops can be the norm. Advanced warning through use of the brake lights can give the operators behind just enough time for them to brake and avoid a rear end collision. Similarly, if a driver’s vehicle were in cruise control and the need to brake arose, it’s vital that the cruise control is disengaged; otherwise fuel would be continually dispensed trying to speed up the vehicle.

PTM Published on: 2014-04-14