Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
TA35-Slide6

The following are unique features of the TA35 1-Pole version. The schematic design shows its use as an ON/OFF switch without overload protection as well as its capability to be used as a 1-pole circuit breaker with thermal overload protection. The voltage on the 1-Pole version is 240VAC and 32VDC.

PTM Published on: 2011-10-17