Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
HIghCap-Slide6

MLCCs have a higher voltage strength. This allows MLCCs to perform better against surge/transient voltages. MLCCs do not require the 2-2.5 times voltage derating rule that is applied to an electrolytic. As an example, in a 10V circuit, the designer can use a 10V rated MLCC as opposed to a 25V rated Tantalum (Ta).

PTM Published on: 2017-08-11