Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
CANAPI-Slide14

In Listen Only Mode, a node does not participate in any communication. It will not acknowledge frames, nor send Error frames. ISO-11898 requires a Listen Only Mode for baud rate detection. Listen Only ensures that a unit just connected to the bus does not affect communication among the other units, until the bus communication speed has been determined and set, and normal communication is possible. The CAN error counters are disabled and the Tx Output is disabled. However, IRR13 is set when a message error occurs. Again, see more in the CAN API application note to learn more about the CAN API!

PTM Published on: 2011-10-25