The RACM1200-V is equipped with many features which can benefit a wide variety of applications. There is an onboard LED that is color and time coded to provide real time feedback on the operating condition of the power supply. The converter is designed for a remote sense that should be connected at the point of load. This is to counteract any voltage drop across long terminal leads. Additionally, the converter features a remote On/Off control, has an adjustable output voltage, and also has two independent outputs: a smart fan output and a standby output.