Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
One of the most common applications for a DC/DC converter is to step down the voltage from a higher voltage source (for example a 24 V industrial power supply) to a lower voltage needed at the load (like a 3.3 V microprocessor).
PTM Published on: 2022-03-23