Shown here is a typical use case for a consumer product that can leverage many of the benefits provided by the i.MX RT1050. The connected autonomous vacuum cleaner is among the many applications that were previously underserved in some capacities by applications processors or MCU products. As shown in the block diagram, while maintaining low cost and development complexity, this product can benefit from various features that are offered by the RT1050, especially the motor control IP leveraged from NXP’s MCU portfolio and the performance improvement without using an application processor.