Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
HDMITFT-Slide3

The HDMI TFT Module Display line consists of twelve TFT modules in 5.0” and 7.0” sizes. These displays come ready to connect with any board or computer capable of HDMI output with a standard HDMI connector cable, and is USB-HID interface ready with a standard micro USB cable. Fit the customers application with one of these 800 x 480 pixel resolution TFTs in Newhaven’s Standard, Premium, or Sunlight Readable version including a resistive, capacitive, or no touch panel. For both the resistive and capacitive touch panel options, USB-HID driver recognition is installed. Each of the touch panel modules are also pre-calibrated in-house to the display they are mounted on. This means that a simple USB to micro-USB cable just needs to be connected from the board with touch interaction output (i.e. RaspberryPi) to the module and the touch interactivity is ready to go immediately.

PTM Published on: 2018-01-09