Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
PIC18F MPLAB Starter Kit Slide 22
The Flash program memory of Microchip’s PIC18F46J50 device is readable, writable and erasable during normal operation over the entire VDD range. This feature gives the user the ability to perform bootloading operations. To demonstrate this feature, the MPLAB Starter Kit for PIC18 comes with a preprogrammed MicroSD card bootloader that gives the ability to load, program, and run PIC18 applications from a MicroSD card. The MicroSD Bootloader accepts user inputs from the capacitive touch buttons and scroll bar and uses the OLED display for user outputs. The MicroSD Bootloader uses substantial parts of the Microchip Memory Disk Drive File System to read files and folders from a MicroSD memory card.
PTM Published on: 2011-10-28