Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
MCU-Slide10

In a typical hybrid application, off-board analog components communicate with the main MCU through common communications interfaces, such as SPI and UART. With this topology, system latency, responsiveness, and performance are often limited by the bottleneck in data transmission speed. With the analog modules on-board, this bottleneck is eliminated as all modules can communicate at “chip speed”. Data is available to be analyzed immediately and, in products with on-board DMA, CPU processing load is minimized.

PTM Published on: 2013-11-29