Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Product List
The performance value table lists the AC Resistance (ACR) and figure of merit (ZTC) when the cold side ceramic is at Tc. If the thermoelectric module’s ACR is in the range in the table, this usually indicates that the module or generator is in good working order. Measuring of the Direct Current Resistance (DCR) cannot be used to determine health since this would activate the cooling/heating effect of the thermoelectric module. ZTC is the ability of a material to efficiently produce thermoelectric power. Both ACR and ZTC are a function of temperature.
PTM Published on: 2018-05-31