Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Functions

If the OVP and OCP settings are lower than the actual voltage/current value, the output of power supply will be turned off. The default settings of the IT6720 are OVP = 61 V, OCP = 5.1 A and the IT6721 OVP = 61 V, OCP = 8.1 A.

PTM Published on: 2023-06-12