Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
DF59S-SN-Slide11

Rated voltages for the DF59S and DF59SN will differ depending on the distance between the two connector sets. For example: Voltages running at 250V need to have a least 2.0mm of space between the two parallel connector sets.

PTM Published on: 2014-08-05