Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
DF40-Slide2

The DF40 series is a space saving FPC to board connector with one of the shortest mating depths in the industry. The connector features a 0.4 mm pitch and 1.5 mm stacking height. The contact area is designed to be protected inside the housing.

PTM Published on: 2009-03-30