Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Associated Content
The 1.25 mm pitch metric pin spacing from the rest of the Gecko range is utilized on the Gecko-MT range for the signal contacts. The pin spacing is 1.25 mm pitch in both rows and columns and is also the same on the PCB Through-board tails.
PTM Published on: 2023-11-14